2024-02-12 6:26 AM - edited 2024-02-14 11:46 PM
I am facing issues while running a BLDC motor using the 6-step algorithm on the STEVAL-SPIN3201 board. The only modification I have made is to the Hall effect sensor low-pass filter to address noisy input signals.
I am encountering the following problems:
Speed fluctuations: The motor speed fluctuates around the reference speed, resulting in uneven current draw (see "1500rpm_no_load.png"). I have tried adjusting the speed regulator tuning to be less aggressive, but this has not resolved the issue.
Current Spikes: Occasional current spikes in the phase currents trigger "Over Current" faults.
Do you have any suggestions on how to address these problems?
The .stwb6 project is included in the Info.zip file
Solved! Go to Solution.
2024-02-23 12:12 AM
Hello @Nikolaj_TL ,
If you have issue with FOC algorithm, please open a new post describing your issue with all required information without considering that part of the information is already in this post. Could you mark the most suitable comment as "Accept as Solution" to close this thread.
Thanks
Cedric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.