2020-07-29 1:22 PM
Several macros in stm32f4xx_hal_exti.h use __LINE__ as a macro parameter. Example:
#define IS_EXTI_PENDING_EDGE(__LINE__) ((__LINE__) == EXTI_TRIGGER_RISING_FALLING)
__LINE__ is a reserved preprocessor symbol which expands to the integer line number of the file in which it is parsed. It should not be used as it is now. F4 HAL library v1.25 (and others).
2020-09-25 10:02 AM
Hi @Charles Miller ,
Even if it is with some delay, it remains relevant to report what you highlighted to our development team. This is what I did.
Thanks,
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.