STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

All the "middlewares" on github. Divide and rule!!

ST has published on github the USBH "middleware" for all MCU families...https://github.com/STMicroelectronics/stm32_mw_usb_hostand LwIP middleware...https://github.com/STMicroelectronics/stm32_mw_lwipand FreeRTOS...https://github.com/STMicroelectroni...

Pavel A. by Super User
  • 886 Views
  • 0 replies
  • 2 kudos

Resolved! Inconsistent HAL_SPI_TransmitReceive Errors

I am running a simple SPI transmit receive project with an STM32F411 (SPI Master) and STM32F303 (SPI Slave). Whenever I press the user push button on the STM32F4 Master, the Master will send a command byte (0xE1) through SPI and the STM32F3 Slave is ...

0693W000001tGAzQAM.png 0693W000001tGB9QAM.png 0693W000001tGBJQA2.png 0693W000001tGBTQA2.png
RrW1 by Associate III
  • 3924 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F072RB and X-CUBE-USB-PD problem.

The usb type c pd example code does not seem to work although it compiles properly using SW4STM32. I tried the provided binary file (PNUCLEO-USB001-DEMO1.bin) and it works just fine. I am using nucleo-f072rb and MB1257 expansion board.PNUCLEO_USB001...

0690X00000BvsUmQAJ.png 0690X00000BvsV1QAJ.png 0690X00000BvsVBQAZ.png 0690X00000BvsVLQAZ.png
Red by Associate II
  • 4708 Views
  • 9 replies
  • 0 kudos

How to resolve an undefined reference to 'end' that is pointing to sysmem.c? C:/Users/dfrancoi/Documents/STMicroelectronics/LwIP_projects/stm32h750b-dk_lwip_V2/Debug/../Src/sysmem.c:57: undefined reference to `end'

I am trying to follow "How to create project for STM32H7 with Ethernet and LwIP stack working" posted on May 29, 2020 however I am getting an error undefined reference to end. When I double click the error it points to sysmem.cNot being an embedded g...

DFran.3 by Associate
  • 1817 Views
  • 0 replies
  • 0 kudos

STM32F7 STM32F769 DFU configuration

Hi,Iam trying to use software DFU bootloader trigger from STM32 application (BOOT1 and BOOT2 are untouchable). Application use USB-FS (service/CDC) and USB-HS (data/CDC), but trigger will be send via existing USB-FS (CDC). USB-FS use PA11 and PA12 an...

embvis by Associate III
  • 2001 Views
  • 3 replies
  • 0 kudos

STM32G071RB USBPD Source auto send Source Cap

STM32G071RB USBPD Source auto send Source Cap when start debug: after reset, I'm not connect cable to C-Type port, I click start debug ( ST-Link ), I send about 50 packet of sourcePlease see in trace and config in attach file

H V N D by Associate III
  • 11619 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.