2017-02-03 7:11 PM
I am using CubeMX with the STM32L4 1.5.2 library. [EDIT -- just confirmed that this exists in 1.6.0 as well]
The non-OTG implementation of HAL_PCDEx_BCD_VBUSDetect() will only call HAL_PCDEx_BCD_Callback() with PCD_BCD_DISCOVERY_COMPLETED if it detects a PCD_BCD_CHARGING_DOWNSTREAM_PORT.
The correct behavior should be to call HAL_PCDEx_BCD_Callback() with PCD_BCD_DISCOVERY_COMPLETED after any type of port is detected.
This is the relevant section of the defective code:
/* If Charger detect ? */
if (USBx->BCDR & USB_BCDR_PDET)
{
/* Start secondary detection to check connection to Charging Downstream
Port or Dedicated Charging Port */
USBx->BCDR &= ~(USB_BCDR_PDEN);
USBx->BCDR |= (USB_BCDR_SDEN);
HAL_Delay(300);
/* If CDP ? */
if (USBx->BCDR & USB_BCDR_SDET)
{
/* Dedicated Downstream Port DCP */
HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DEDICATED_CHARGING_PORT);
}
else
{
/* Charging Downstream Port CDP */
HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_CHARGING_DOWNSTREAM_PORT);
/* Battery Charging capability discovery finished
Start Enumeration*/
HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DISCOVERY_COMPLETED);
}
}
else /* NO */
{
/* Standard Downstream Port */
HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_STD_DOWNSTREAM_PORT);
}
This is what a correctly working version looks like:
/* If Charger detect ? */
if (USBx->BCDR & USB_BCDR_PDET)
{
/* Start secondary detection to check connection to Charging Downstream
Port or Dedicated Charging Port */
USBx->BCDR &= ~(USB_BCDR_PDEN);
USBx->BCDR |= (USB_BCDR_SDEN);
HAL_Delay(300);
/* If CDP ? */
if (USBx->BCDR & USB_BCDR_SDET)
{
/* Dedicated Downstream Port DCP */
HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DEDICATED_CHARGING_PORT);
}
else
{
/* Charging Downstream Port CDP */
HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_CHARGING_DOWNSTREAM_PORT);
}
}
else /* NO */
{
/* Standard Downstream Port */
HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_STD_DOWNSTREAM_PORT);
}
/* Battery Charging capability discovery finished
Start Enumeration*/
HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DISCOVERY_COMPLETED);
As an aside, it would be helpful if STM's HAL libraries were hosted in a public git repo so one could file a bug report and provide a pull request for the fix, rather than having to post this sort of thing in a public forum. It is ill suited for reporting and fixing software defects.
#usb #bcd #stm32l4We’re moving the ST Community to a new platform to give you a better and more reliable community experience.