2026-01-15 1:47 AM - last edited on 2026-01-15 1:53 AM by mƎALLEm
Hi,
I got stuck in the HardFault_Handler every time after editing some code.
I'm using FreeRTOS in c++ combination with classes. First I thought this would be a memory issue.
After increasing configTOTAL_HEAP_SIZE and configMINIMAL_STACK_SIZE, I was still stuck in the HardFault_Handler. Even by jumping into a function, before I returned from this function the HardFault_Handler was tripped again.
I really tried a number of things...
I made a function (bool Controller::DefaultConfig()) to set the default configuration when nothing was available in the flash and I forgot the return true or false. When adding the return with a result, the problem with HardFault was solved.
Is this a logical behavior? (A compiler error would make more sense)
Greetings,
ErX
Solved! Go to Solution.
2026-01-15 3:44 AM
@ErX wrote:I made a function (bool Controller::DefaultConfig()) to set the default configuration when nothing was available in the flash and I forgot the return true or false. When adding the return with a result, the problem with HardFault was solved.
Is this a logical behavior? (A compiler error would make more sense)
You should get a compiler warning for this, but you may need to enable it in the project's settings.
As you are probably already aware, not having a return statement leads to undefined behaviour - which is one of the things that can lead to a hard fault being signalled.
2026-01-15 2:18 AM
Hello,
How to debug a HardFault on an Arm® Cortex®-M STM32
2026-01-15 2:19 AM
There is a fault analyzer in STM32CubeIDE and STM32Cube VS Code extension (Fault Status Register View) that gives you detailed insight about what exactly happened.
Segger has excellent stuff here Cortex-M Fault - SEGGER Knowledge Base.
FreeRTOS has options to get stack usage high watermarks during runtime (uxTaskGetStackHighWaterMark, uxTaskGetStackHighWaterMark2 - FreeRTOS™).
hth
KnarfB
2026-01-15 2:36 AM
In addition to the STM32-specific link from @mƎALLEm, here are some more general Cortex-M resources:
https://community.arm.com/support-forums/f/embedded-forum/3257/debugging-a-cortex-m0-hard-fault
2026-01-15 3:44 AM
@ErX wrote:I made a function (bool Controller::DefaultConfig()) to set the default configuration when nothing was available in the flash and I forgot the return true or false. When adding the return with a result, the problem with HardFault was solved.
Is this a logical behavior? (A compiler error would make more sense)
You should get a compiler warning for this, but you may need to enable it in the project's settings.
As you are probably already aware, not having a return statement leads to undefined behaviour - which is one of the things that can lead to a hard fault being signalled.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.