2025-12-10 3:51 AM - edited 2025-12-10 4:21 AM
Hi ST Team,
I need to implement USB Host Printer support on STM32F767 using USBX.
I'm trying to send PCL6 (HP LaserJet) print jobs via USB.
Challenge: No Host Printer example exists in stm32-usbx-examples
(only Device Printer and Host MSC/CDC).
What I need:
1. Is USBX Host Printer class available? Any code?
2. How to send binary PCL6 data to printer (USB Bulk OUT)?
3. CubeMX configuration for USB Host (FS/HS)?
4. Printer enumeration and status read examples?
5. Any complete working reference project?
Current Setup:
- STM32F767ZI + FreeRTOS + USBX
- HP LaserJet printer (USB)
- Using HP's jetlib for PCL6 generation
Please advise or point to relevant docs/code.
Thanks,
Madhu07
2025-12-10 6:38 AM
hello @MADHU2
Well USBX host printer class is available. However, So far, no example is provided to cover Printer class as far as I know. CubeMX imports Middleware files and leaves it to developer to tailor their application in app_usbx_host.c/h.
you can check USBX middleware
here is some threads that can help you thread1 thread2 thread3
for cubeMX configuration just ensure that you are sending a clean 48mhz to the USB and you are using the correct pins you can check your product datasheet. You can also review AN4879
Hope that helps for now, I will come back to you if I find any other information
Gyessine
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.