STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F429ZI ETH_MACMIIAR CR: max value?

STM32F429ZI Ethernet @180MHzRM0090 33.8.1 page 1197, ETH_MACMIIAR CR: max value is 100 150-168MHz HCLK/102Is this a print error (other micros in the family can only reach 168MHz) or the controller is not specified to work at 180MHz ?Thx

scaprile by Associate III
  • 4824 Views
  • 4 replies
  • 0 kudos

Compilation error of Ux_Host_MSC example

Moved from this thread. Why does attempting to compile this example result in these errors?     ../../USBX/Target/ux_stm32_config.h:29:10: fatal error: stm32h5xx_hal.h: No such file or directory 29 | #include "stm32h5xx_hal.h" | ^~~~~~~~~~~~~~~~~  ...

custom bootloader on STM32F446

Hi everybody,I'm trying to make a bootloader in my STM32F446. The aim if this one is the possibility to update the firmware but with keeping the previous one in case of issue. So, I'll have two slots for firmware.For now, I have the following sectors...

fab04 by Senior
  • 673 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.