2026-02-11 9:15 AM - last edited on 2026-02-11 10:10 AM by Andrew Neil
Hi,
on STM32F429I-DISC the timer TIM2 kicks ADC1 and the data goes to buffer via DMA. APB1 clock for TIM2 is 36MHz, reload value for TIM2 is 143, I exspect 36e6/144= 250k samples/second.
I get 8.3e6 samples in 123 seconds which results in 67.4ks/s. This is factor 3.7 low, not even an integer ratio.
There is a clock issue for the 48MHz, see enclosed .ioc
What do I miss?
THX Cheers
Detlef
2026-02-15 10:14 PM
> I get 8.3e6 samples in 123 seconds which results in 67.4ks/s.
Measured how exactly? Be precise.
The timings provided in the Reference Manual are correct, so you need to present enough information to be able to spot the error.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.