STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo-H723zg - Continuous ADC with DMA issues

 Hello, I have a Nucleo-H723ZG that I am trying to setup a Continuous running ADC that fills a buffer VIA DMA. I have read tutorials, watched videos, looked at the data sheets and still can't get it working.Tools:  CubeMX to generate code   VScode to...

Screenshot_2026-02-12_20-09-05.png Screenshot_2026-02-12_20-08-35.png Screenshot_2026-02-12_20-08-16.png
Uvamosk by Associate II
  • 399 Views
  • 5 replies
  • 0 kudos

Resolved! Inaccurate signal frequency measurement using TIM

Hi, I'm using STM32F407 TIM1 channel 1 to measure the frequency of a square wave. The result is not accurate. For example, when input frequency is 1000.0Hz, the result is around 1006Hz. Input frequency has been verified by an oscilloscope, with probe...

fzl by Associate II
  • 1142 Views
  • 16 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.