2025-04-29 7:41 AM
Hallo all:
I want to implement a generic counter to count the number of impulses on an input, but after debouncing.
I guess that mechanical switches for human interface purposes need a debouncing in the milliseconds range, say 1 ms to 20 ms. My Systick interrupt runs every millisecond, so I can sample the input there (with an appropriate prescaler implemented in software), which should take care of debouncing.
If the input comes from a clean, high-speed signal, I can use a hardware timer like TIM1 in order to count impulses on input TIM1_CH1. I can do some level of debouncing with its built-in hardware input filter, but if the signal is clean, then probably no debouncing is necessary.
The trouble is at mid input frequencies. I am thinking of some signal source which is faster than switches typical for human interfaces, but not completely clean (with some bouncing). Is that a plausible scenario at all?
I am using an STM32F407. I have set APB1 to its maximum speed of 42 MHz, and APB2 to 84 Mhz. This way, I can drive SPI interfaces, high-resolution timers etc. at a very high speed or with great precision.
The STM32 timer input filters are ultimately clocked from tCK_INT, which is APB1 or APB2, depending on the timer. Unfortunately, there is no prescaler there, so tCK_INT gets the full 84 MHz in my case. You can scale a little down with CKD, so that tDTS = 4 × tCK_INT. You can then set the filter to fSAMPLING=fDTS/32, N=8. That means I can scale the filter frequency down a factor of to 4 * 32 = 128, in my case 84 MHz / 128 = around 656 kHz, but no further. With a sample count of N = 8, this means I can filter down to a stability period of 12 us. But not further, say to 50 us.
So the question is, how to debounce the input signal in the frequency range 1 Khz - 656 kHz, for stability periods 1000 us to 12 us.
I could increase the Systick frequency in order to sample the input more often in software, but if I increase it too much, general firmware performance would suffer.
I could use a dedicated timer interrupt just to sample the input more often in software, but again, if interrupts come too often, general firmware performance would suffer.
I could strongly reduce the frequency for APB1 and/or APB2, but then other peripherals would be affected. At the very least, I would have to adjust the timing parameters in all my firmware, which is a lot of work.
Is there any other way to sample an input quickly in hardware, at regular intervals?
Can I use a hardware timer to trigger some automatic sampling? Would I need to use DMA to store the input into a memory buffer? Can I have that buffer automatically wrap around?
Another way is to implement debouncing in hardware, with a simple low-pass filter, but then the debouncing time wouldn't be configurable in software.
Thanks in advance,
rdiez
Solved! Go to Solution.
2025-04-29 2:07 PM
There's no magic solution here. Other chips have more options available for TIM sources. If you are debouncing buttons pressed by a human, polling them at 1 kHz and debouncing in software is more than sufficient.
Any system which interrupts the chip on each edge could overwhelm the system with interrupts, so not advised.
2025-04-29 9:02 AM
Do you have another free 32-bit timer?
If yes, you could configure this to count with 1 µs, no interrupts (maybe overflow as info), ARR set to 32-bit max. Just let it run free in the background.
Each time you sample the IO / whatever, also save the current 1us-tick-time = CNT, and so on ...
2025-04-29 2:07 PM
There's no magic solution here. Other chips have more options available for TIM sources. If you are debouncing buttons pressed by a human, polling them at 1 kHz and debouncing in software is more than sufficient.
Any system which interrupts the chip on each edge could overwhelm the system with interrupts, so not advised.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.