2021-01-25 10:10 AM
I'm using nucleo f429zi with LWIP v 2.1.2. Documentation states that for TX buffer PBUF_RAM should be used. In my case whole LWIP stack freeze after 28 send messages. When I change pbuf type to PBUF_POOL, everything works like a charm. Although in the docs it written that this type should be used for RX buffer. Here is my implementation of udp callback function.
void
udp_descserver_receive_callback(void *arg, struct udp_pcb *upcb, struct pbuf *p, const ip_addr_t *addr, u16_t port) {
uint8_t triesNumber = 0;
err_t error;
udp_connect(upcb, addr, port);
pbuf_free(p);
p = NULL;
p = pbuf_alloc(PBUF_TRANSPORT, sizeof(PING_INFO), PBUF_POOL);
if(p != NULL) {
pbuf_take(p, &pingInfo, sizeof(PING_INFO));
do {
error = udp_send(upcb, p);
triesNumber++;
} while (error && triesNumber < RESEND_TRIES);
}
pbuf_free(p);
udp_disconnect(upcb);
}Also I get message "Assertion failed p != NULL"
My question is, why the method which is contrary to docs works.
2021-01-25 10:18 AM
Well that looks prone to die if p is NULL
I'd definitely do something different on line 17 to stop it freeing a NULL pointer.
Are the allocation routines thread safe?
2021-01-25 10:56 AM
I could move line 17th inside IF statement. I think they should be I only use one thread, no OS.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.