2016-04-20 3:25 AM
Hello,
In order to send SERIAL_STATE over USB IN interrupt endpoint I had to increase the CDC_CMD_PACKET_SIZE to 10 in usbd_cdc.h. Is there a way to do this in cubemx ? I'd like to keep my modification at each code regeneration. By the way, if someone is interrested to send SERIAL_STATE here are my modifications : In usb_cdc_if.h add in USER CODE BEGIN EXPORTED_TYPES: typedef union { uint8_t val; struct{ unsigned dcd :1; unsigned dsr :1; unsigned break_err :1; unsigned ri :1; unsigned frame_err :1; unsigned parity_err :1; unsigned overrun_err :1; unsigned reserved :1; }; } USBD_CDC_SerialStateTypeDef; and in USER CODE BEGIN EXPORTED_FUNCTIONS:uint8_t CDC_Serial_State(USBD_CDC_SerialStateTypeDef serial_state);
In usb_cdc_if.h add in USER CODE BEGIN PRIVATE_VARIABLES:uint8_t CDC_Serial_State_Buf[10] = {
0xA1, // vmRequestType 0x20, // SERIAL_STATE 0x00, // wValue 0x00, 0x00, // wIndex 0x00, 0x02, // wLength 0x00, 0x00, // UART state bitmap 0x00, }; and add in USER CODE BEGIN PRIVATE_FUNCTIONS_IMPLEMENTATION (I know It's not private but there is no public user code section) :/**
* @brief CDC_Serial_State * Send SERIAL_STATE over USB IN interrupt endpoint through this function. * @note * * * @param serial_state: Uart State Bitmap Value * @retval Result of the operation: USBD_OK if all operations are OK else USBD_FAIL or USBD_BUSY */ uint8_t CDC_Serial_State(USBD_CDC_SerialStateTypeDef serial_state) { USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*)hUsbDevice_0->pClassData; if (hcdc->TxState != 0){ return USBD_BUSY; } CDC_Serial_State_Buf[8] = serial_state.val; hUsbDevice_0->ep0_state = USBD_EP0_STATUS_IN; hUsbDevice_0->ep_in[0].total_length = 10; hUsbDevice_0->ep_in[0].rem_length = 10; /* Start the transfer */ USBD_LL_Transmit (hUsbDevice_0, CDC_CMD_EP, CDC_Serial_State_Buf, 10); return USBD_OK; } For the moment it is only tested with RING state, on a small demo project with a stm32l4dicovery. All improvement proposals or comments are welcome. Regards, #usb-cdc-serial_state2016-04-20 8:23 AM
Hi Stany MARCEL,
Your question will be forwarded to our MX team for further checks.Then thanks for sharing your solution.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-10-11 2:22 AM
Dear user,
Unfortunately there is no solution to your problem for now. Indeed STM32CubeMX, inherits the file usb_cdc.h as a copy from STM32Cube firmware package.
We consider it as an enhancement of our solution.
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.