STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

32F3 USB without HSE

Posted on June 22, 2016 at 08:40How can one use the USB without HSE oscillator? I have been playing with the STM32F3 discovery board, on the original preloaded firmware there is USB functionality, but the board doesn't have any external oscillator p...

STM32F302

Posted on September 06, 2016 at 18:15http://www.compel.ru/infosheet/ST/STM32F302R6T6STM32F302 CAN and USB at the same time?We are thinking of using an STM32F302R6T6  KB for our next project. But I need to know if CAN and USB can be used at the same ...

ssurneed by Associate II
  • 1046 Views
  • 1 replies
  • 0 kudos

HAL I2C

Posted on September 06, 2016 at 13:59Hello friends. I'm having difficulty with the work via a I2C interface using the STM32 HAL Library. Microcontroller STM32 F205RG. The project generated STM32CubeMX. The problem is this: in debug mode or after pro...

[HELP]STM32F4-DISCOVERY with MP3 Player

Posted on March 02, 2016 at 08:02Hei thereIs there any working mp3 player using this eval board ?Right now I try helix mp3 decoder but cannot compile using keil v4.There are some error on assembly.h i cannot understand.Please guide me thanks. #mp...

dree86 by Associate II
  • 8204 Views
  • 16 replies
  • 0 kudos

Run Nucleo only with power, no PC USB connection

Posted on September 01, 2016 at 18:33Hy, I start to work with the Nucleo Platform. I have several Nucleos and can program them with System Workbench for STM32, no problem. But when I connect the USB cable to either a USB power pack or a PC that has ...

harald by Associate III
  • 1791 Views
  • 2 replies
  • 0 kudos

Problem with ethernet

Posted on August 31, 2016 at 10:23Hi, I'm using STM32F746-DISCOVERY. I want to use ethernet, but I connect for a little time 3-4 seconds and the the connection dropped. When I try to connect again I cant. I saw the example of ST and there isn't any ...

STM32F1 USB interrupts, why LP and HP?

Posted on August 30, 2016 at 13:11Given that in some instances both interrupts can be active at the same time, what is the point or use in having two? Is there any reason why the vector table for both shouldn't point to the same interrupt routine su...

Mikexx by Associate II
  • 2571 Views
  • 1 replies
  • 1 kudos

USB Init fails on AHB Idle not set

Posted on August 29, 2016 at 19:43STM32F427.I cloned a cube project for a working application with Micrium os.  I want to run code without an OS.  As far as I can tell so far I am doing all the same initializations but the function USB_CoreReset fai...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.