2016-10-11 2:54 AM
Hello I am trying to use the ADC like this:
ADC_ChannelConfTypeDef sConfig; adc.Instance = ADC1; adc.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4; adc.Init.Resolution = ADC_RESOLUTION_12B; adc.Init.ScanConvMode = DISABLE; adc.Init.ContinuousConvMode = DISABLE; adc.Init.DiscontinuousConvMode = DISABLE; adc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; adc.Init.DataAlign = ADC_DATAALIGN_RIGHT; adc.Init.NbrOfConversion = 1; adc.Init.DMAContinuousRequests = DISABLE; adc.Init.EOCSelection = ADC_EOC_SINGLE_CONV; if (HAL_ADC_Init(&adc) != HAL_OK) { //Error_Handler(); } sConfig.Channel = ADC_CHANNEL_0; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES; if (HAL_ADC_ConfigChannel(&adc, &sConfig) != HAL_OK) { //Error_Handler(); }GPIO_InitTypeDef GPIO_InitStruct; if(adcHandle->Instance==ADC1) { __HAL_RCC_ADC1_CLK_ENABLE(); GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_4; GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5); }HAL_ADC_Start
(
&
g_AdcHandle
)
;
for
(
;
;
)
{
if
(
HAL_ADC_PollForConversion
(
&
g_AdcHandle
,
1000000
)
==
HAL_OK
)
{
g_ADCValue
=
HAL_ADC_GetValue
(
&
g_AdcHandle
)
;
g_MeasurementNumber
++
;
}
}
But it gets stuck in this code, looking for EOC flag:while(!(__HAL_ADC_GET_FLAG(hadc, ADC_FLAG_EOC))) { /* Check if timeout is disabled (set to infinite wait) */ if(Timeout != HAL_MAX_DELAY) { if((Timeout == 0U) || ((HAL_GetTick() - tickstart ) > Timeout)) { /* Update ADC state machine to timeout */ SET_BIT(hadc->State, HAL_ADC_STATE_TIMEOUT); /* Process unlocked */ __HAL_UNLOCK(hadc); return HAL_TIMEOUT; } } }Any ideas why this happens? #adc #hal2016-10-11 10:00 AM
I managed to solve this, Part of my code was executing in an interrupt and this was blocking the EOC flag from getting set, after I moved it out, it worked great.
2016-10-11 11:16 AM
Hi paulstrom.bjorn,
Thank you for sharing your finding . You can manage the interrupt conflict by setting the priorities of each interrupt in the NVIC register to be executed by priority's order and avoid such issue.-Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.