2016-10-10 9:29 AM
Hi, I generated project in CubeMX, and I can't run ETH. Connections to PHY are fine. My program run on line 215 in file stm32f1xx_hal_eth.c whitch is:
while (((heth->Instance)->DMABMR & ETH_DMABMR_SR) != (uint32_t)RESET) { }I read errata for that MCU, and it is said, that it is possible, that DMA is not working after changing power mode for sleep or stop, but I am not doing it in code, and eth DMA seems to be enabled. Please help me anyone. #dma #eth #eth_dmabmr2016-10-10 2:02 PM
MII/RMII clock running? All 3 clock enable bits in RCC set?
JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.