2017-09-28 6:01 AM
Greetings , I'm currently trying to adapt raw LWIP example code for the STM32F769I Board for use on my STM32F767ZI , I'm a novice and wanted to know if anyone can provide assistance with regards to this .
#nucleof7 #raw-lwip2017-09-28 6:18 AM
Hello,
You have various choices, regarding the way to start in order to develop your application:
- You can review LwIP examples as you can find available in the STM32CubeF7 package relevant to your device. It can help you as an implementation example to develop your own application:
STM32Cube_FW_F7_V1.8.0\Projects\STM32F767ZI-Nucleo\Applications\LwIP
- You can start your own application using CubeMX to initialize peripherals you need with the configuration you want.
Also, you may re-use sections available in the Cube examples or get inspired from them.
The reference manual provides complete information on how to use the STM32F7xx microcontroller memory and peripherals.
Have a look to these documents:- UM1709, it maybe helpful as it provides a full description of how to implement In-Application Programming (IAP) using Ethernet communication.- UM1713 : STM32Cube interfacing with LwIP and examples.- UM1718: paragraph 'B.3.6 LwIP' for the STM32CubeMX LwIP side.
- AN3966 : “LwIP TCP/IP stack demonstration for STM32F4x7 microcontrollers�
Otherwise, if you have any problem, you can share your issue and code on the community with details, this will help user forum to help you.
Kind Regards
Imen
2017-09-28 7:30 AM
>>I'm a novice and wanted to know if anyone can provide assistance with regards to this .
For commercial needs, ST also maintains a list of consultants and contractors.
Porting code is a fairly standard practice, pay attention to the details regarding components, pins and clocks.
2017-09-28 10:19 AM
My use of the board is not commercial .I'm a student trying to use board for my final project. So figuring it out is pretty much part of my course.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.