2019-05-27 4:11 AM
I want to customize System memory UART Boot-loader and will use as Flash Memory Boot-loader. Please share the System memory Boot-loader Source code or the link where it is available.
Regards
Vijendra
2019-05-27 5:24 AM
Even if you get sources, you cannot patch the system memory bootloader. It is not rewritable.
-- pa
2019-05-27 5:27 AM
I don't want to rewrite it in system memory. I will use as flash memory bootloader .
2019-05-27 5:37 AM
You are on the wrong track.
Forget about the ROM-based system bootloader. Even if you pay ST dearly, it is of no worth for your endeavor.
You want a second-stage bootloader, which is just viewed as a normal application during system start.
There are plenty of examples available for several STM32 types, not sure about L071.
2020-12-14 4:28 AM
I submitted an "Idea" to ST, asking them to publish bootloader source code.
If you're also interested in the bootloader sources, be sure to vote on the idea: https://community.st.com/s/ideazone#0873W000000PAwtQAG
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.