cancel
Showing results for 
Search instead for 
Did you mean: 

RTC init fails after CLOSED→OPEN regression on STM32H563 with TrustZone

JWagner
Associate

Using on a STM32H563RI with trustzone for a secure bootloader and non-secure application. Both the secure and non-secure side were correctly working in OPEN state, and I did a test of going to a CLOSED state and regression back to OPEN with authenticated debug. After the regression, RTC_EnterInitMode(), times out trying to enter init mode and HAL_RTC_Init() fails. I tried the solution from this form post of calling HAL_PWR_EnableBkUpAccess() and that did not work.

Notes:

- Trustzone and the secure watermarks for the bootloader were reprogrammed in the option bytes after regression.

- RTC is LSI as its clock source.

- The call to HAL_RCCEx_PeriphCLKConfig() in HAL_RTC_MspInit() returns HAL_OK.

- The RTC pheripheral is marked non-secure.

- The code has not been changed since preforming the regression and was working previously.

 

The RTC Init Code and Clock configs are included below.

void MX_RTC_Init(void)
{

  /* USER CODE BEGIN RTC_Init 0 */

  /* USER CODE END RTC_Init 0 */

  RTC_PrivilegeStateTypeDef privilegeState = {0};

  /* USER CODE BEGIN RTC_Init 1 */

  /* USER CODE END RTC_Init 1 */

  /** Initialize RTC Only
  */
  hrtc.Instance = RTC;
  hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
  hrtc.Init.AsynchPrediv = 127;
  hrtc.Init.SynchPrediv = 255;
  hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
  hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
  hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
  hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
  hrtc.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE;
  hrtc.Init.BinMode = RTC_BINARY_NONE;
  if (HAL_RTC_Init(&hrtc) != HAL_OK)
  {
    Error_Handler();
  }
  privilegeState.rtcPrivilegeFull = RTC_PRIVILEGE_FULL_NO;
  privilegeState.backupRegisterPrivZone = RTC_PRIVILEGE_BKUP_ZONE_NONE;
  privilegeState.backupRegisterStartZone2 = RTC_BKP_DR0;
  privilegeState.backupRegisterStartZone3 = RTC_BKP_DR0;
  if (HAL_RTCEx_PrivilegeModeSet(&hrtc, &privilegeState) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN RTC_Init 2 */

  /* USER CODE END RTC_Init 2 */

}

void HAL_RTC_MspInit(RTC_HandleTypeDef* rtcHandle)
{

  RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
  if(rtcHandle->Instance==RTC)
  {
  /* USER CODE BEGIN RTC_MspInit 0 */

  /* USER CODE END RTC_MspInit 0 */

  /** Initializes the peripherals clock
  */
    PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RTC;
    PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;
    if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
    {
      Error_Handler();
    }

    /* RTC clock enable */
    __HAL_RCC_RTC_ENABLE();
    __HAL_RCC_RTCAPB_CLK_ENABLE();
  /* USER CODE BEGIN RTC_MspInit 1 */

  /* USER CODE END RTC_MspInit 1 */
  }
}

void SystemClock_Config(void)
{
    RCC_OscInitTypeDef RCC_OscInitStruct = { 0 };
    RCC_ClkInitTypeDef RCC_ClkInitStruct = { 0 };

    /** Configure the main internal regulator output voltage
     */
    __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);

    while (!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY))
    {
    }

    /** Initializes the RCC Oscillators according to the specified parameters
     * in the RCC_OscInitTypeDef structure.
     */
    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI | RCC_OSCILLATORTYPE_HSE;
    RCC_OscInitStruct.HSEState       = RCC_HSE_ON;
    RCC_OscInitStruct.LSIState       = RCC_LSI_ON;
    RCC_OscInitStruct.PLL.PLLState   = RCC_PLL_ON;
    RCC_OscInitStruct.PLL.PLLSource  = RCC_PLL1_SOURCE_HSE;
    RCC_OscInitStruct.PLL.PLLM       = 6;
    RCC_OscInitStruct.PLL.PLLN       = 125;
    RCC_OscInitStruct.PLL.PLLP       = 2;
    RCC_OscInitStruct.PLL.PLLQ       = 5;
    RCC_OscInitStruct.PLL.PLLR       = 2;
    RCC_OscInitStruct.PLL.PLLRGE     = RCC_PLL1_VCIRANGE_2;
    RCC_OscInitStruct.PLL.PLLVCOSEL  = RCC_PLL1_VCORANGE_WIDE;
    RCC_OscInitStruct.PLL.PLLFRACN   = 0;
    if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
    {
        Error_Handler();
    }

    /** Initializes the CPU, AHB and APB buses clocks
     */
    RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1 |
                                  RCC_CLOCKTYPE_PCLK2 | RCC_CLOCKTYPE_PCLK3;
    RCC_ClkInitStruct.SYSCLKSource   = RCC_SYSCLKSOURCE_PLLCLK;
    RCC_ClkInitStruct.AHBCLKDivider  = RCC_SYSCLK_DIV1;
    RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
    RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
    RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;

    if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
    {
        Error_Handler();
    }

    /** Configure the programming delay
     */
    __HAL_FLASH_SET_PROGRAM_DELAY(FLASH_PROGRAMMING_DELAY_2);
}

void PeriphCommonClock_Config(void)
{
    RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = { 0 };

    /** Initializes the peripherals clock
     */
    PeriphClkInitStruct.PeriphClockSelection =
        RCC_PERIPHCLK_USART1 | RCC_PERIPHCLK_USART2 | RCC_PERIPHCLK_SPI2 | RCC_PERIPHCLK_SPI3;
    PeriphClkInitStruct.PLL2.PLL2Source      = RCC_PLL2_SOURCE_HSE;
    PeriphClkInitStruct.PLL2.PLL2M           = 3;
    PeriphClkInitStruct.PLL2.PLL2N           = 20;
    PeriphClkInitStruct.PLL2.PLL2P           = 15;
    PeriphClkInitStruct.PLL2.PLL2Q           = 4;
    PeriphClkInitStruct.PLL2.PLL2R           = 2;
    PeriphClkInitStruct.PLL2.PLL2RGE         = RCC_PLL2_VCIRANGE_3;
    PeriphClkInitStruct.PLL2.PLL2VCOSEL      = RCC_PLL2_VCORANGE_WIDE;
    PeriphClkInitStruct.PLL2.PLL2FRACN       = 0;
    PeriphClkInitStruct.PLL2.PLL2ClockOut    = RCC_PLL2_DIVP | RCC_PLL2_DIVQ;
    PeriphClkInitStruct.Usart1ClockSelection = RCC_USART1CLKSOURCE_PLL2Q;
    PeriphClkInitStruct.Usart2ClockSelection = RCC_USART2CLKSOURCE_PLL2Q;
    PeriphClkInitStruct.OspiClockSelection   = RCC_OSPICLKSOURCE_PLL1Q;
    PeriphClkInitStruct.Spi2ClockSelection   = RCC_SPI2CLKSOURCE_PLL2P;
    PeriphClkInitStruct.Spi3ClockSelection   = RCC_SPI3CLKSOURCE_PLL2P;
    if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
    {
        Error_Handler();
    }
}

 

3 REPLIES 3
Jocelyn RICARD
ST Employee

Hello @JWagner ,

I understand you have following use case:

1) close the device : code is working fine

2) run authenticated debug (not regression) to reopen the device without erasing the firmware

3) attach the debugger and run and face issue with RTC

My first guess would be that you attach to the target and debug the non secure application.

In such case you have to make sure that you first execute the secure part to setup everything correctly.

What could happen is that you only reset the non secure while it was already running, which could explain what you see.

Please force the system reset. If you have external reset button, run debugger and reset, you should stop at beginning of the main of the non secure. In such case, everything should work.

Best regards

Jocelyn

 

JWagner
Associate

Hi Jocelyn,

The case is works fine in open. Works fine in closed, but once I do a full regression from closed back to open and reinstall the same secure and non-secure firmware, the RTC init fails. The firmware has not changed. Is there a option byte related to the RTC or anything else that in the peripheral that changes on a regression that would not be re-enabled by the firmware. I am setting all my option bytes as I had them configured previously.

Jocelyn RICARD
ST Employee

Hello @JWagner ,

I don't know what happens. I suspect RTC being stuck.

Is your device using a battery connected to RTC?

Did you try a power-on reset?

Best regards

Jocelyn

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.