2025-02-13 6:03 AM - last edited on 2025-02-13 6:05 AM by Andrew Neil
I'm working with the STM32F769 microcontroller and I've defined a new section in the linker script using instructions from https://www.openstm32.org/Using%2BCCM%2BMemory :
/* Emulated RAM in the JPEG peripheral */
HACK_RAM_JPEG_HUFFENC_AC0 (rwx): ORIGIN = 0x40024000, LENGTH = 352 /* JPEG->HUFFENC_AC0 */
.hackRamJpegHuffencAc0 :
{
. = ALIGN(4);
KEEP(*(.hackRamJpegHuffencAc0))
*(.hackRamJpegHuffencAc0 .hackRamJpegHuffencAc0.*)
} >HACK_RAM_JPEG_HUFFENC_AC0
/* Used by the startup to initialize data */
_sidata_HACK_RAM_JPEG_HUFFENC_AC0 = LOADADDR(.data_HACK_RAM_JPEG_HUFFENC_AC0);
/* Initialized HACK_RAM_JPEG_HUFFENC section
*
* IMPORTANT NOTE!
* If initialized variables will be placed in this section,
* the startup code needs to be modified to copy the init-values.
*/
.data_HACK_RAM_JPEG_HUFFENC_AC0 :
{
. = ALIGN(4);
_sdata_HACK_RAM_JPEG_HUFFENC_AC0 = .; /* create a global symbol at data start */
*(.data_HACK_RAM_JPEG_HUFFENC_AC0) /* .data sections */
*(.data_HACK_RAM_JPEG_HUFFENC_AC0*) /* .data* sections */
. = ALIGN(4);
_edata_HACK_RAM_JPEG_HUFFENC_AC0 = .; /* define a global symbol at data end */
} >HACK_RAM_JPEG_HUFFENC_AC0 AT> FLASH
/* Uninitialized (bss-like) section in HACK_RAM_JPEG_HUFFENC_AC0 */
.bss_HACK_RAM_JPEG_HUFFENC_AC0 :
{
. = ALIGN(4);
_sbss_HACK_RAM_JPEG_HUFFENC_AC0 = .; /* Define the start of bss */
*(.bss.HACK_RAM_JPEG_HUFFENC_AC0) /* Uninitialized section */
*(.bss.HACK_RAM_JPEG_HUFFENC_AC0.*)
. = ALIGN(4);
_ebss_HACK_RAM_JPEG_HUFFENC_AC0 = .; /* Define the end of bss */
} >HACK_RAM_JPEG_HUFFENC_AC0
I have absolutely no knowledge of assembler programming and ChatGPT was just hallucinating when I asked him, so I don't know how to change the assembler code in startup_stm32f769xx.s. Unlike in the example (https://www.openstm32.org/Using%2BCCM%2BMemory ), I'm adding a section, not replacing a section. So, can somebody please help me to modify startup_stm32f769xx.s so that __HAL_RCC_JPEG_CLK_ENABLE() is called and then the HACK_RAM_JPEG_HUFFENC_AC0 area is initialized?
Solved! Go to Solution.
2025-02-13 8:02 AM
I solved it by calling a regular C-function (placed inside a C-file) from the assembler code:
.extern InitHackMemory /* Declare external C function */
LoopFillZerobss:
ldr r3, = _ebss
cmp r2, r3
bcc FillZerobss
/* Call the clock system intitialization function.*/
bl SystemInit
/* Call static constructors */
bl __libc_init_array
/* Call the external C function to initialize hack memory */
bl InitHackMemory
/* Call the application's entry point.*/
bl main
bx lr
.size Reset_Handler, .-Reset_Handler
// External symbols from linker script
extern uint32_t _sidata_HACK_RAM_JPEG_HUFFENC_AC0;
extern uint32_t _sdata_HACK_RAM_JPEG_HUFFENC_AC0;
extern uint32_t _edata_HACK_RAM_JPEG_HUFFENC_AC0;
extern uint32_t _sbss_HACK_RAM_JPEG_HUFFENC_AC0;
extern uint32_t _ebss_HACK_RAM_JPEG_HUFFENC_AC0;
void InitHackMemory(void) {
__HAL_RCC_JPEG_CLK_ENABLE();
uint32_t *src=&_sidata_HACK_RAM_JPEG_HUFFENC_AC0;
uint32_t *dst = &_sdata_HACK_RAM_JPEG_HUFFENC_AC0;
// Copy initialized data from Flash to RAM
while (dst < &_edata_HACK_RAM_JPEG_HUFFENC_AC0) {
*dst++ = *src++;
}
// Zero initialize the .bss section
while (dst < &_ebss_HACK_RAM_JPEG_HUFFENC_AC0) {
*dst++ = 0;
}
}
2025-02-13 8:02 AM
I solved it by calling a regular C-function (placed inside a C-file) from the assembler code:
.extern InitHackMemory /* Declare external C function */
LoopFillZerobss:
ldr r3, = _ebss
cmp r2, r3
bcc FillZerobss
/* Call the clock system intitialization function.*/
bl SystemInit
/* Call static constructors */
bl __libc_init_array
/* Call the external C function to initialize hack memory */
bl InitHackMemory
/* Call the application's entry point.*/
bl main
bx lr
.size Reset_Handler, .-Reset_Handler
// External symbols from linker script
extern uint32_t _sidata_HACK_RAM_JPEG_HUFFENC_AC0;
extern uint32_t _sdata_HACK_RAM_JPEG_HUFFENC_AC0;
extern uint32_t _edata_HACK_RAM_JPEG_HUFFENC_AC0;
extern uint32_t _sbss_HACK_RAM_JPEG_HUFFENC_AC0;
extern uint32_t _ebss_HACK_RAM_JPEG_HUFFENC_AC0;
void InitHackMemory(void) {
__HAL_RCC_JPEG_CLK_ENABLE();
uint32_t *src=&_sidata_HACK_RAM_JPEG_HUFFENC_AC0;
uint32_t *dst = &_sdata_HACK_RAM_JPEG_HUFFENC_AC0;
// Copy initialized data from Flash to RAM
while (dst < &_edata_HACK_RAM_JPEG_HUFFENC_AC0) {
*dst++ = *src++;
}
// Zero initialize the .bss section
while (dst < &_ebss_HACK_RAM_JPEG_HUFFENC_AC0) {
*dst++ = 0;
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.