2025-06-23 10:17 PM - last edited on 2025-06-24 12:37 AM by Peter BENSCH
I am working on a project using the STM32H743ZI microcontroller.
I want to implement SPI communication using the LL (Low-Layer) drivers instead of HAL.
:question_mark: Can you confirm whether the STM32H743ZI supports LL SPI driver APIs like LL_SPI_Init, LL_SPI_TransmitData8, etc.?
Also, are there any specific settings or header files (like USE_FULL_LL_DRIVER) required to enable these LL functions in STM32CubeIDE
Does STM32H743ZI support SPI communication using LL drivers? I’m using STM32CubeIDE.
SPI1 is enabled, but LL_SPI functions are disabled unless I define USE_FULL_LL_DRIVER.
Is this the correct way to enable LL SPI support?
2025-06-25 10:14 PM
hi I am trying to stm32cube ide ,Enable the LL _spi but stm32h7xx_ll_spi.h file not enable the functions . why ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.