STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U5 File system with FreeRTOS

Hello,I'm using NucleoU575 with CubeMx and I want to make a file system on my SD card.I want to use FreeRtos but there are no Fatfs in CubeMx and the FileX cannot work with FreeRtos (image). Is there anyway i can use Fatfs with STM32U5 ?Thank you. 

_legacyfs_online_stmicro_images_0693W00000bk2bEQAQ.png
M326.1 by Associate II
  • 9225 Views
  • 6 replies
  • 2 kudos

Encrypted DFU Custom Bootloader

Hello,What is the simplest and best way to implement encrypted firmware update via DFU?  I plan on building a custom bootloader but have not found any recent existing projects.  I tried STM32-AES-Bootloader but it is setup for STM32F10 and I am using...

LMorr.3 by Senior II
  • 1261 Views
  • 1 replies
  • 0 kudos

STM32U5 sleep

hi all,i am developing a project using stm32u585 microcontroller which can connect to the external devices using ethernet and USB protocols.i need to put the controller in sleep or any low power mode when ever a sleep command is reached through the U...

sabari1 by Associate III
  • 3186 Views
  • 3 replies
  • 0 kudos

Resolved! Problem communicating with bootloader on STM32F7

Hello, I am trying to use one MCU to program another MCU, both of which are STM32 F746ZG boards.Let the MCU that is sending the commands be MCU 1, and the MCU in the bootloader mode be MCU2.I use the following command in the MCU2 to start its default...

is45_0-1750677679135.png
is45 by Associate III
  • 1238 Views
  • 4 replies
  • 5 kudos

Resolved! RTC Issue

Hello Community!I have an issue with reading / writing the RTC in an H723 MCU.The issue is:I can set the Clock to a date, but when I read out the RTC, then the year is 10 years in the future.e.g. I set the time to now (2025 / 06 / 22 19:mm:ss) and I ...

CBerg by Senior II
  • 1495 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.