2018-06-26 2:00 PM
Hello All,
I hope your doing good. I am working on a project based on STM32L476RG using Keil v5. I have used assert in my code. It works correctly for the compiler optimization L2 and L3. But when I change to Level 1 or 0, i get
'G3\G3.axf: Error: L6218E: Undefined symbol __aeabi_assert (referred from st_spi.o).'
Anybody with any leads on this. Thank you all for your time.
Muthaiah Murugappan
#optimization #hal-spi #stm32l4762018-06-26 2:15 PM
See this link:
http://www.keil.com/support/man/docs/armlib/armlib_chr1358938924063.htm
Apparently with the Keil compiler the assert() macro behaves differently depending on the optimization level. The real question is why the linker isn't finding the __atabi_assert() function that is supposed to be in a library somewhere.
2018-06-26 2:48 PM
Hello Bob,
Thanks for getting back to me. The link you sent describes a better picture for my issue. Thanks for the information.
Even I'm not able to figure out, why the compiler doesn't find out the library function.
Thanks
Muthaiah Murugappan
2018-06-26 5:21 PM
>>Even I'm not able to figure out, why the compiler doesn't find out the library function.
Keil has support contact numbers for such issues.
2018-06-27 8:11 AM
Hey Clive, thanks for responding, I will get in touch with keil support and post an update here.
2018-06-27 10:49 AM
Are there portions of the project that aren't getting rebuilt properly, or pulled in as libraries?
Have you tried Rebuild-All?
2018-06-27 12:54 PM
Yes Clive, I have tried rebuilding all and I guess there isn't portions, not getting rebuilt properly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.