STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PlatformIO stm32cube framework isn't complete

Posted on May 16, 2018 at 19:54I am using https://platformio.org/platformio-ide to program the STM32 F7 discovery board. The STM32Cube package is in the PlatformIO's framework registry and HAL&CMSIS drivers are working out of the box without problem...

Jur Div by Associate II
  • 1649 Views
  • 1 replies
  • 0 kudos

ADC STM32F746 precision problem

Posted on May 17, 2018 at 14:02hello everyone,i've been trying to find the right configuration for my stm in order to acquire data from a ct sensor (ECS 1030) but i can't find the right configuration i've done some tests, i got a sampled signal that...

Resolved! Default Bootloader Source

Posted on May 15, 2018 at 19:21I'm working with a NUCLEO-F411RE and am starting to look at writing a custom bootloader. Is the default bootloader source available somewhere that I could use as a reference?#stm32-bootloader

Konami by Senior II
  • 3054 Views
  • 6 replies
  • 0 kudos

Create two TCP servers on stm32

Posted on May 15, 2018 at 15:38Hello,I'm trying to create two TCP servers on the STM32F767ZI microcontroller. I created my first server which is a WEB server (port 80). And now I would like to add a second TCP server (port 502). I created a second t...

0690X0000060KhRQAU.png 0690X0000060Kd1QAE.png 0690X0000060KhgQAE.png

DfuSe fails to upload to write-protected chip

Posted on May 14, 2018 at 20:16Hi!I'm using STM32F105RB chip with built-in bootloader code (jumping to bootloader by selecting BOOT0/BOOT1 voltages)If part of the chip is write protected then chip erase fails , and the MCU eventually reboots into it...

yury by Associate II
  • 725 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.