2025-04-10 9:53 PM - last edited on 2025-05-09 4:06 AM by Sarra.S
Hello ST Community & @stforum & @stforum2
I am working on a project using the STM32F765VGT6 MCU with STM32CubeIDE on Windows, and I'm implementing a Custom HID USB interface.
Objective:
To send more than 16 bytes of data over USB using the `USBD_CUSTOM_HID_SendReport()` function.
USB Report Descriptor (Working - 16 Bytes):
__ALIGN_BEGIN static uint8_t CUSTOM_HID_ReportDesc_FS[USBD_CUSTOM_HID_REPORT_DESC_SIZE] __ALIGN_END =
{
0x06, 0x00, 0xFF, // USAGE_PAGE (Vendor Defined Page: 0xFF00)
0x09, 0x01, // USAGE (Vendor Defined)
0xA1, 0x01, // COLLECTION (Application)
// Output Report (16 bytes)
0x85, 0xE3, // REPORT_ID (227)
0x09, 0x01,
0x15, 0x00,
0x25, 0x01,
0x75, 0x08,
0x95, 0x10, // REPORT_COUNT = 16
0xB1, 0x03, // FEATURE (Data, Var, Abs)
// Input Report (16 bytes)
0x85, 0xE4, // REPORT_ID (228)
0x09, 0x02,
0x15, 0x00,
0x25, 0xFF,
0x75, 0x08,
0x95, 0x10, // REPORT_COUNT = 16
0x81, 0x02, // INPUT (Data, Var, Abs)
0xC0 // END_COLLECTION
};
#define USBD_CUSTOMHID_OUTREPORT_BUF_SIZE 16U
#define USBD_CUSTOM_HID_REPORT_DESC_SIZE 32U
#define CUSTOM_HID_EPIN_ADDR 0x81U
#define CUSTOM_HID_EPIN_SIZE 0x40U
#define CUSTOM_HID_EPOUT_ADDR 0x01U
#define CUSTOM_HID_EPOUT_SIZE 0x40U
Modified Descriptor for 32 Bytes (Not Working):
// Output Report (32 bytes)
0x85, 0xE3,
0x09, 0x01,
0x15, 0x00,
0x25, 0x01,
0x75, 0x08,
0x95, 0x20, // REPORT_COUNT = 32
0xB1, 0x03,
// Input Report (32 bytes)
0x85, 0xE4,
0x09, 0x02,
0x15, 0x00,
0x25, 0xFF,
0x75, 0x08,
0x95, 0x20, // REPORT_COUNT = 32
0x81, 0x02,
For 32 bytes and 64 bytes unable to transmit the data and sometimes device not detecting
Thanks
Badrinathan J
Solved! Go to Solution.
2025-05-09 8:44 AM
Hi @Badrinathan
Did you update buffer size?
#define USBD_CUSTOMHID_OUTREPORT_BUF_SIZE 32U
Ensure that the buffer sizes in your configuration match the report size.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-09 8:44 AM
Hi @Badrinathan
Did you update buffer size?
#define USBD_CUSTOMHID_OUTREPORT_BUF_SIZE 32U
Ensure that the buffer sizes in your configuration match the report size.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.