2024-08-16 12:14 PM
Hello, all. I am currently trying to program a black pill board to print out the output from a sound sensor, for which I use the Arduino IDE 2.3.2.
Used components:
- STM32F411CEU6 black pill
- KY-037 sound sensor
Current connections:
- the "G" pin from the sensor is connected to the "GND" pin on the black pill
- the "+" pin from the sensor is connected to the "3v3" pin on the black pill
- the "A0" pin from the sensor is connected to the "A9" pin on the black pill
The code:
#define DIGITAL_INPUT PA9
void setup() {
Serial.begin(9600);
pinMode(DIGITAL_INPUT, INPUT);
}
void loop() {
Serial.println(analogRead(DIGITAL_INPUT));
}
This code prints out values around 270-290 and it doesn't seem like creating any loud noises has any effect on the output, and neither does changing the potentiometer on the sensor itself. What I am trying to get is an output that has a clear and visible change between different amounts of noise. I am starting to think that the current output is just the floating value of the "A9" pin.
Other relevant info:
- I believe the problem isn't in the black pill itself, since I can successfully implement a simple "blink" functionality.
- I have already adjusted the potentiometer on the sensor so that the L2 is off. It turns on briefly when it detects a noise (such as clapping or anything louder).
- Changing the pin from "A9" outputs values from different ranges, but those values still don't seem to be affected by any noise, no matter how loud.
- The values don't change if "A9" is connected to the "A0" pin on the sensor instead of "D0".
If anyone can offer some assistance, I would majorly appreciate it.
Solved! Go to Solution.
2024-08-17 2:41 PM
I double-checked the contact on the black pill pins and it seems that it fixed the issue. Apparently the contacts on all the pins were a bit weak, so I reinforced them a bit and now I am getting an actual output. Now I get values around 690 in silence, with different jumps in value depending on the sounds I make. I can't believe it was such a trivial thing afterall.
I appreciate you all helping me out and I wish you the best of luck in your future endeavors. Have a great day!
2024-08-16 12:17 PM
Quick correction for the last point in other relevant info. The values don't change if "A9" is connected to the "D0" pin on the sensor instead of "A0".
2024-08-17 5:35 AM
The sensors seems to.give high or low. So you should not use analog read. Chek with a multimeter if the output changes. https://www.arduino.cc/reference/en/language/functions/digital-io/digitalread/
2024-08-17 7:47 AM
Hi , you need to use an analog pin
2024-08-17 9:44 AM
I already am. Is A9 not analog?
2024-08-17 9:47 AM
What do you mean "high or low"? The sensor has both an analog output pin and a digital one. If I use digitalRead, I just get a constant output of "0", even when I can clearly see that L2 is on.
2024-08-17 12:01 PM
@robotics_beginner wrote:I already am. Is A9 not analog?
2024-08-17 2:41 PM
I double-checked the contact on the black pill pins and it seems that it fixed the issue. Apparently the contacts on all the pins were a bit weak, so I reinforced them a bit and now I am getting an actual output. Now I get values around 690 in silence, with different jumps in value depending on the sounds I make. I can't believe it was such a trivial thing afterall.
I appreciate you all helping me out and I wish you the best of luck in your future endeavors. Have a great day!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.