2021-08-09 3:26 AM
After 36, it will give error and exited from code.
I tried another card , the code will set the sector count to 16 and loops through it to make the read complete. As i am trying a large file, its taking so much time.
I just want to know, is the sector count ( 16 and 64 for the 2 cards) is solely dependent on card and whether i can change from code. What is the relevance of sector 36 if sector count is 64. Anybody please clarify these things...
Attached code for reference. Above I refer( 64 and 16) the value of cc in file ff.c ( line no.3557)
Thanks,
Jestina
2021-08-09 10:52 AM
Could it relate to the cluster size being used by the file system on specific cards?
Perhaps look at those via "Properties" in Windows, or the metrics FatFs can provide.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.