2024-06-25 1:32 AM
MCU: STM32L072CZx
Development Board: B-L072Z-LRWAN1
Middleware: USB-RNDIS From STM32's GitHib: STM32_MW_USB_DEVICE.
Entire Project for SMT32CubeIDE is attached as Attachment.
I have Integrated the USB-RNDIS Middleware Stack into the Project using STM32CubeIDE.
Below are my List of Issues:
I also Installed the USBView on System to Check the Endpoints and Other Parameters, Not Sure what am I missing, But I see some Issue on USBView.
Below are the Details From USBView Tool:
[Port3] : USB to Ethernet Adapter
Is Port User Connectable: yes
Is Port Debug Capable: no
Companion Port Number: 16
Companion Hub Symbolic Link Name: USB#ROOT_HUB30#4&3329762&0&0#{f18a0e88-c30c-11d0-8815-00a0c906bed8}
Protocols Supported:
USB 1.1: yes
USB 2.0: yes
USB 3.0: no
---===>Device Information<===---
String Descriptor for index 2 not available while device is in low power state.
ConnectionStatus:
Current Config Value: 0x00 -> Device Bus Speed: Full (is not SuperSpeed or higher capable)
Device Address: 0x16
Open Pipes: 0
*!*ERROR: No open pipes!
===>Device Descriptor<===
bLength: 0x12
bDescriptorType: 0x01
bcdUSB: 0x0200
bDeviceClass: 0x02
*!*ERROR: device class should be Multi-interface Function 0xEF
When IAD descriptor is used
bDeviceSubClass: 0x02 -> This is the Common Class Sub Class
bDeviceProtocol: 0x00
*!*ERROR: device Protocol should be USB IAD Protocol 1
When IAD descriptor is used
bMaxPacketSize0: 0x40 = (64) Bytes
idVendor: 0x0FE6 = Sospita ASA
idProduct: 0x9700
bcdDevice: 0x0200
iManufacturer: 0x01
String Descriptor for index 1 not available while device is in low power state.
iProduct: 0x02
String Descriptor for index 2 not available while device is in low power state.
iSerialNumber: 0x03
String Descriptor for index 3 not available while device is in low power state.
bNumConfigurations: 0x01
---===>Full Configuration Descriptor<===---
===>Configuration Descriptor<===
bLength: 0x09
bDescriptorType: 0x02
wTotalLength: 0x004B -> Validated
bNumInterfaces: 0x02
bConfigurationValue: 0x01
iConfiguration: 0x00
bmAttributes: 0xC0 -> Self Powered
MaxPower: 0x32 = 100 mA
===>IAD Descriptor<===
bLength: 0x08
bDescriptorType: 0x0B
bFirstInterface: 0x00
bInterfaceCount: 0x02
bFunctionClass: 0xE0
*!*CAUTION: This appears to be an invalid Interface Class
bFunctionSubClass: 0x01
bFunctionProtocol: 0x03
iFunction: 0x00
===>Interface Descriptor<===
bLength: 0x09
bDescriptorType: 0x04
bInterfaceNumber: 0x00
bAlternateSetting: 0x00
bNumEndpoints: 0x01
bInterfaceClass: 0x02 -> This is Communications (CDC Control) USB Device Interface Class
bInterfaceSubClass: 0x02
bInterfaceProtocol: 0xFF
iInterface: 0x00
-> This is a Communications (CDC Control) USB Device Interface Class
===>Descriptor Hex Dump<===
bLength: 0x05
bDescriptorType: 0x24
05 24 00 10 01
-> This is a Communications (CDC Control) USB Device Interface Class
===>Descriptor Hex Dump<===
bLength: 0x05
bDescriptorType: 0x24
05 24 01 00 01
-> This is a Communications (CDC Control) USB Device Interface Class
===>Descriptor Hex Dump<===
bLength: 0x04
bDescriptorType: 0x24
04 24 02 00
-> This is a Communications (CDC Control) USB Device Interface Class
===>Descriptor Hex Dump<===
bLength: 0x05
bDescriptorType: 0x24
05 24 06 00 01
===>Endpoint Descriptor<===
bLength: 0x07
bDescriptorType: 0x05
bEndpointAddress: 0x82 -> Direction: IN - EndpointID: 2
bmAttributes: 0x03 -> Interrupt Transfer Type
wMaxPacketSize: 0x0010 = 0x10 bytes
bInterval: 0x10
===>Interface Descriptor<===
bLength: 0x09
bDescriptorType: 0x04
bInterfaceNumber: 0x01
bAlternateSetting: 0x00
bNumEndpoints: 0x02
bInterfaceClass: 0x0A -> This is a CDC Data USB Device Interface Class
bInterfaceSubClass: 0x00
bInterfaceProtocol: 0x00
iInterface: 0x00
===>Endpoint Descriptor<===
bLength: 0x07
bDescriptorType: 0x05
bEndpointAddress: 0x01 -> Direction: OUT - EndpointID: 1
bmAttributes: 0x02 -> Bulk Transfer Type
wMaxPacketSize: 0x0040 = 0x40 bytes
bInterval: 0x00
===>Endpoint Descriptor<===
bLength: 0x07
bDescriptorType: 0x05
bEndpointAddress: 0x81 -> Direction: IN - EndpointID: 1
bmAttributes: 0x02 -> Bulk Transfer Type
wMaxPacketSize: 0x0040 = 0x40 bytes
bInterval: 0x00
@Hana Slimi@ALABSTM, Team Please Support on this.
2024-06-27 5:38 AM
The Issue I had earlier mentioned, i.e.
>> It Gets Detected on Linux Platform and is also Enabled, Unfortunately Post a Specific Number of Packets (i.e. ~ 70-85 Packets) the Code Runs into a HardFault_Handler.
This has been fixed, The Fix was as below
In the Source File, usbd_cdc_rndis_if_template.c, Under Function, CDC_RNDIS_Itf_Receive(uint8_t *Buf, uint32_t *Len), I had to Set the UserRxBuffer and not &Buf[0]
i.e. USBD_CDC_RNDIS_SetRxBuffer(&hUsbDeviceFS,UserRxBuffer);
But Now, I see another issue, i.e. The Data received is not as what is being sent. I see it as
Issue with Window's being disabled still persists
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.