STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2S audio crackly noise on STM32L05x

Hello everyone!I am struggling with playback via I2S to external DAC on STM32L051/53. Audio:file in external SPI flash,WAV format16KHz sampling rate16bit depthI run the core on internal oscillator. My 'real' I2S clock (WS frequency) is 15,957kHz, whi...

MBank.1 by Associate II
  • 5916 Views
  • 8 replies
  • 0 kudos

USBH_BulkReceiveData not working

Hello everybody,I am currently trying to implement a RTL2832 on STM32, the initialisation process works just fine (USBH_CtlReq). But during the USBH_RTLSDR_Process, my program first uses a USBH_BulkReceiveData and loops on USBH_LL_GetURBState. the st...

ABouk.1 by Associate III
  • 852 Views
  • 0 replies
  • 0 kudos

Fail to find serial connected ST microcontroller device (integrating a STM32L475VET6) via windows api functions (SetupDiGetClassDevs, SetupDiEnumDeviceInterfaces) on some windows 7/8/10 systems

Hello,I maintain the firmware und update software of a device that integrates a ST microcontroller (STM32L475VET6). The update software is implemented in javascript and c++. In windows 7/8/10 the update software sometimes fails to find the device uti...

AGroe.1 by Associate II
  • 2525 Views
  • 4 replies
  • 0 kudos

Resolved! Facing linking error Error[Lp015]: section placement failure: overcommitted content in [0x2000'0020-0x2000'0028] while running x-cube-classb-v2-3-0 with IAR 8.40.1

Hi Sir/Madam,I'm trying to compile x-cube-classb-v2-3-0 STM32G081B_Eval project in IAR 8.40.1 but it giving below linker error.Error[Lp015]: section placement failure: overcommitted content in [0x2000'0020-0x2000'0028] It is compiling fine with IAR 8...

Anitha by Associate III
  • 8057 Views
  • 5 replies
  • 0 kudos

Resolved! How to use HAL_SD_WriteBlocks_DMA

I'm working on a project that requires USB_OTG_FS and USB_DEVICE as MSC; I've managed to hook up the SD card to the USB_DEVICE layer and the HAL_SD_ReadBlocks works fine and I can even play back music from the SD Card via the MSC interface. However t...

DMagy.1 by Associate
  • 2563 Views
  • 1 replies
  • 0 kudos

Voice recorder with STM32F7 as .wav and on SD card

I want to make voice recorder with STM32F7 and save voice as .wav in SD card. before this one, i tried to save audio samples as .txt file, but during save them in sd card by FAT, some sample has been lost. therefore i try to another way. Please help ...

MMosa.1 by Associate II
  • 4732 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.