2024-09-05 4:39 AM
HI,
I am trying to interface the USB device with a customized STM32H563ZIT6 controller board. I followed the example steps from the STM Community, but the USB port is not detected. What should I do?
Anyway, I will upload my project. Please verify it
Solved! Go to Solution.
2024-09-24 4:04 AM
I would add that if you need any recommendations about Hardware design you can refer to the board provided schematics. https://www.st.com/resource/en/schematic_pack/mb1404-h563zi-c01-schematic.pdf
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-05 5:15 AM
First of all, get (buy, rent, steal) a real hardware USB analyzer, to see what is actually transmitted on the wires.
When the electric layer is good you can use software USB analyzers.
2024-09-05 9:10 PM
@Pavel A.Are there any other methods? When I verified the USB interface with the STM32F429ZIT6 controller, I did not use any analyzer.
2024-09-06 5:33 AM
If the electrical interface has been validated, next step: capture USB traffic, act based on observations. Does enumeration begin at all?
2024-09-24 4:04 AM
I would add that if you need any recommendations about Hardware design you can refer to the board provided schematics. https://www.st.com/resource/en/schematic_pack/mb1404-h563zi-c01-schematic.pdf
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.