STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 high latency with usb hid game controller

Hi, I'm using an stm32f102 for making usb game controller (custom hid) with 29 buttons. The problem is, that the latency if I check on PC is feelable, too high. I made some tests to figure out the problem, but I don't have any idea yet. If I just re...

BPoko by Associate
  • 4159 Views
  • 4 replies
  • 0 kudos

STM32H743VIT6 can't connect with a LAN8720!

I have WeAct STM32H743 (STM32H743VIT6 ) and I can't connect it with a LAN8720 module!I did all my steps according by example from this link https://www.st.com/en/embedded-software/stm32cubeh7.html But, it doesn't help me!How to find out at what stage...

DK.7 by Senior
  • 3811 Views
  • 5 replies
  • 0 kudos

Resolved! Test for EDATA FLASH ECC code on STM32H563

Hello All,We are looking into testing our code that access the EDATA and handle FLASH ECCC (single bit error) and ECCD (double bit error).How can we simulate those errors?Is it possible to insert single bit or double bit errors using a JTAG? It would...

L_P by Associate II
  • 4254 Views
  • 7 replies
  • 5 kudos

Resolved! Watermark in Azure ThreadX?

Greetings and thanks for reading.  FreeRTOS has a built in utility function uxTaskGetStackHighWaterMark() that reports on the amount of space unused by the stack.   You can use this function to gauge just how much of the stack is used and how close y...

flash erase fail

hello:      I use STM32H7A3VGT6 in our board, two flash regions are available in the MCU and their start address are 0x08000000 and 0x08080000, all in bank1, when I use STM32CubeProgrammer to erase more than 3 sectors from 0x08080000, it works well, ...

lbapplem by Associate II
  • 2604 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.