2016-05-30 4:21 AM
Hi, I have emulated two VCPs with only one USB Device. I can send data in one VCP that has the following Endpoint Address.
#define CDC_IN_EP 0x81 /* EP1 for data IN */#define CDC_OUT_EP 0x01 /* EP1 for data OUT */#define CDC_CMD_EP 0x82 /* EP2 for CDC commands */
I would like to know if it's possible to send data in the other VCP with other Endpoint Address like :
#define CDC_IN_EP3 0x83 /* EP3 for data IN */#define CDC_OUT_EP3 0x03 /* EP3 for data OUT */#define CDC_CMD_EP4 0x84 /* EP4 for CDC commands */
My problem is that addresses others than 0x81 don't allow me to send data over the second VCP. I'm using two CDC interfaces Full-Speed. Normally we can use 7 endpoints with CDC_FS and that's what I'm trying to do.. I have 6 Endpoints: 3 for each VCP and the seventh is Endpoint 0 for configuration.
Have I missed something in the Endpoints Configuration or in the Composite Device Descriptors ?
Thank you guys.
#composite #usb #stm32 #device2016-05-31 7:02 AM
Hi el_alaoui.moulay_has,
USB CDC does not allow more than one IN endpoint at single Communication Data class interface.Information mentioned in :
-
Enumeration as CDC device with 2 data endpoints (IN and OUT) and 1 command endpoint (IN)
-
http://cscott.net/usb_dev/data/devclass/usbcdc11.pdf
, p12:3.4.2 Data Class Endpoint Requirements
The type of endpoints belonging to a Data Class interface are restricted to being either isochronous or bulk, and are expected to exist in pairs of the same type (one In and one Out).
-Hannibal-
2016-06-01 12:04 AM
Thank you Hannibal,
I read the Document. You said ''Yes you can have more than one In Bulk data endpoint, and the number of total endpoints depends of the device you are using
'' I have 2 CDC interfaces that leads to use 2 Data Class Interfaces (Because I'm emulating two Virtual COM Ports) so I can use 2 IN Bulk endpoints to transmit and receive data in these two VCPs. When I use 0x81 address for the first IN Bulk Endpoint I can transmit and receive data in the first Virtual COM Port, but when I use (0x82/0x83/0x84/0x85/0x86) addresses for the other IN Bulk Endpointit doesn't work. (I use STM32F4 Discovery Board). Here are my descriptors for the two Interface Association Descriptors (IAD) :/* USB CDC device Configuration Descriptor */__ALIGN_BEGIN uint8_t USBD_CDC_CfgFSDesc[USB_CDC_CONFIG_DESC_SIZ] __ALIGN_END ={
/*Configuration Descriptor*/
0x09, /* bLength: Configuration Descriptor size */
USB_DESC_TYPE_CONFIGURATION, /* bDescriptorType: Configuration */
USB_CDC_CONFIG_DESC_SIZ, /* wTotalLength:no of returned bytes */
0x00,
0x04, /* bNumInterfaces: 4 interface */
0x01, /* bConfigurationValue: Configuration value */
0x00, /* iConfiguration: Index of string descriptor describing the configuration */
0xC0, /* bmAttributes: self powered */
0x32, /* MaxPower 100 mA */
/*---------------------------------------------------------------------------*/
// IAD0
0x08, // bLength: Interface Descriptor size
0x0B, // bDescriptorType: IAD
0x00, // bFirstInterface
0x02, // bInterfaceCount
0x02, // bFunctionClass: CDC
0x02, // bFunctionSubClass
0x01, // bFunctionProtocol
0x02, // iFunction
/*Interface0 Descriptor */
0x09, /* bLength: Interface Descriptor size */
USB_DESC_TYPE_INTERFACE, /* bDescriptorType: Interface */
/* Interface descriptor type */
0x00, /* bInterfaceNumber: Number of Interface */
0x00, /* bAlternateSetting: Alternate setting */
0x01, /* bNumEndpoints: One endpoints used */
0x02, /* bInterfaceClass: Communication Interface Class */
0x02, /* bInterfaceSubClass: Abstract Control Model */
0x01, /* bInterfaceProtocol: Common AT commands */
0x00, /* iInterface: */
/*Header Functional Descriptor*/
0x05, /* bLength: Endpoint Descriptor size */
0x24, /* bDescriptorType: CS_INTERFACE */
0x00, /* bDescriptorSubtype: Header Func Desc */
0x10, /* bcdCDC: spec release number */
0x01,
/*Call Management Functional Descriptor*/
0x05, /* bFunctionLength */
0x24, /* bDescriptorType: CS_INTERFACE */
0x01, /* bDescriptorSubtype: Call Management Func Desc */
0x03, /* bmCapabilities: D0+D1 */
0x01, /* bDataInterface: 1 */
/*ACM Functional Descriptor*/
0x04, /* bFunctionLength */
0x24, /* bDescriptorType: CS_INTERFACE */
0x02, /* bDescriptorSubtype: Abstract Control Management desc */
0x02, /* bmCapabilities */
/*Union Functional Descriptor*/
0x05, /* bFunctionLength */
0x24, /* bDescriptorType: CS_INTERFACE */
0x06, /* bDescriptorSubtype: Union func desc */
0x00, /* bMasterInterface: Communication class interface */
0x01, /* bSlaveInterface0: Data Class Interface */
/*Endpoint 2 Descriptor*/
0x07, /* bLength: Endpoint Descriptor size */
USB_DESC_TYPE_ENDPOINT, /* bDescriptorType: Endpoint */
CDC_CMD_EP, /* bEndpointAddress */
0x03, /* bmAttributes: Interrupt */
LOBYTE(CDC_CMD_PACKET_SIZE), /* wMaxPacketSize: */
HIBYTE(CDC_CMD_PACKET_SIZE),
0xFF, /* bInterval: */
/*---------------------------------------------------------------------------*/
/*Data class interface descriptor*/
0x09, /* bLength: Endpoint Descriptor size */
USB_DESC_TYPE_INTERFACE, /* bDescriptorType: */
0x01, /* bInterfaceNumber: Number of Interface */
0x00, /* bAlternateSetting: Alternate setting */
0x02, /* bNumEndpoints: Two endpoints used */
0x0A, /* bInterfaceClass: CDC */
0x00, /* bInterfaceSubClass: */
0x00, /* bInterfaceProtocol: */
0x00, /* iInterface: */
/*Endpoint OUT Descriptor*/
0x07, /* bLength: Endpoint Descriptor size */
USB_DESC_TYPE_ENDPOINT, /* bDescriptorType: Endpoint */
CDC_OUT_EP, /* bEndpointAddress */
0x02, /* bmAttributes: Bulk */
LOBYTE(CDC_DATA_FS_MAX_PACKET_SIZE), /* wMaxPacketSize: */
HIBYTE(CDC_DATA_FS_MAX_PACKET_SIZE),
0x00, /* bInterval: ignore for Bulk transfer */
/*Endpoint IN Descriptor*/
0x07, /* bLength: Endpoint Descriptor size */
USB_DESC_TYPE_ENDPOINT, /* bDescriptorType: Endpoint */
CDC_IN_EP, /* bEndpointAddress */
0x02, /* bmAttributes: Bulk */
LOBYTE(CDC_DATA_FS_MAX_PACKET_SIZE), /* wMaxPacketSize: */
HIBYTE(CDC_DATA_FS_MAX_PACKET_SIZE), 0x00, /* bInterval: ignore for Bulk transfer */
/*---------------------------------------------------------------------------*/
// IAD1
0x08, // bLength: Interface Descriptor size
0x0B, // bDescriptorType: IAD
0x02, // bFirstInterface
0x02, // bInterfaceCount
0x02, // bFunctionClass: CDC
0x02, // bFunctionSubClass
0x01, // bFunctionProtocol
0x02, // iFunction
/*Interface1 Descriptor */
0x09, /* bLength: Interface Descriptor size */
USB_DESC_TYPE_INTERFACE, /* bDescriptorType: Interface */
/* Interface descriptor type */
0x02, /* bInterfaceNumber: Number of Interface */
0x00, /* bAlternateSetting: Alternate setting */
0x01, /* bNumEndpoints: One endpoints used */
0x02, /* bInterfaceClass: Communication Interface Class */
0x02, /* bInterfaceSubClass: Abstract Control Model */
0x01, /* bInterfaceProtocol: Common AT commands */
0x00, /* iInterface: */
/*Header Functional Descriptor*/
0x05, /* bLength: Endpoint Descriptor size */
0x24, /* bDescriptorType: CS_INTERFACE */
0x00, /* bDescriptorSubtype: Header Func Desc */
0x10, /* bcdCDC: spec release number */
0x01,
/*Call Management Functional Descriptor*/
0x05, /* bFunctionLength */
0x24, /* bDescriptorType: CS_INTERFACE */
0x01, /* bDescriptorSubtype: Call Management Func Desc */
0x03, /* bmCapabilities: D0+D1 */
0x03, /* bDataInterface: 1 */
/*ACM Functional Descriptor*/
0x04, /* bFunctionLength */
0x24, /* bDescriptorType: CS_INTERFACE */
0x02, /* bDescriptorSubtype: Abstract Control Management desc */
0x02, /* bmCapabilities */
/*Union Functional Descriptor*/
0x05, /* bFunctionLength */
0x24, /* bDescriptorType: CS_INTERFACE */
0x06, /* bDescriptorSubtype: Union func desc */
0x02, /* bMasterInterface: Communication class interface */
0x03, /* bSlaveInterface0: Data Class Interface */
/*Endpoint 2 Descriptor*/
0x07, /* bLength: Endpoint Descriptor size */
USB_DESC_TYPE_ENDPOINT, /* bDescriptorType: Endpoint */
CDC_CMD_EP4, /* bEndpointAddress */
0x03, /* bmAttributes: Interrupt */
LOBYTE(CDC_CMD_PACKET_SIZE), /* wMaxPacketSize: */
HIBYTE(CDC_CMD_PACKET_SIZE),
0xFF, /* bInterval: */
/*---------------------------------------------------------------------------*/
/*Data class interface descriptor*/
0x09, /* bLength: Endpoint Descriptor size */
USB_DESC_TYPE_INTERFACE, /* bDescriptorType: */
0x03, /* bInterfaceNumber: Number of Interface */
0x00, /* bAlternateSetting: Alternate setting */
0x02, /* bNumEndpoints: Two endpoints used */
0x0A, /* bInterfaceClass: CDC */
0x00, /* bInterfaceSubClass: */
0x00, /* bInterfaceProtocol: */
0x00, /* iInterface: */
/*Endpoint OUT Descriptor*/
0x07, /* bLength: Endpoint Descriptor size */
USB_DESC_TYPE_ENDPOINT, /* bDescriptorType: Endpoint */
CDC_OUT_EP3, /* bEndpointAddress */
0x02, /* bmAttributes: Bulk */
LOBYTE(CDC_DATA_FS_MAX_PACKET_SIZE), /* wMaxPacketSize: */
HIBYTE(CDC_DATA_FS_MAX_PACKET_SIZE),
0x00, /* bInterval: ignore for Bulk transfer */
/*Endpoint IN Descriptor*/
0x07, /* bLength: Endpoint Descriptor size */
USB_DESC_TYPE_ENDPOINT, /* bDescriptorType: Endpoint */
CDC_IN_EP3, /* bEndpointAddress */
0x02, /* bmAttributes: Bulk */
LOBYTE(CDC_DATA_FS_MAX_PACKET_SIZE), /* wMaxPacketSize: */
HIBYTE(CDC_DATA_FS_MAX_PACKET_SIZE),
0x00 /* bInterval: ignore for Bulk transfer */
};
Have I missed something in the Endpoints Configuration or in the Composite Device Descriptors ?
Thank you Hannibal.
2016-09-19 7:21 AM
Hi el_alaoui.moulay_has,
I recommend these both thread that contains guidelines and explanation about composite device's project building which may help you to figure out what you have missed. [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Multiple%20USB%20CDC%20%28USB%20IAD%%20How¤tviews=9776]Thread1 -Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.