2023-08-17 10:24 PM
Hello,
Recently I try to use the CRC unit insde stm32h753vih6 to do the crc calculation. According to the spec(RM0433), I tried to read/write the registers defined in chapter21. But all the five CRC related registers(CRC_DR, CRC_IDR, CRC_CR, CRC_INIT, CRC_POL) are zero and cannot be changed.
addr:0x58024c00 value:0x0
addr:0x58024c04 value:0x0
addr:0x58024c08 value:0x0
addr:0x58024c0c value:0x0
addr:0x58024c10 value:0x0 //CRC_POL should have 0x04c11db7 as the default value
I have tried to reset CRC unit through CRC_CR bit0. But the issue still exists.
Does CRC module need extra configuration so that it can be used?
Solved! Go to Solution.
2023-08-18 12:35 AM - edited 2023-08-18 12:36 AM
I think that I just find out the rootcause. I didn't call __HAL_RCC_CRC_CLK_ENABLE() to enable the CRC clock. After doing that, I can access the CRC related registers.
2023-08-17 10:34 PM
In the beginning, I followed the following example to do the crc calculation but always got the zero crc value. Then I tried to access its registers and then got the issue described in my post.
2023-08-18 12:35 AM - edited 2023-08-18 12:36 AM
I think that I just find out the rootcause. I didn't call __HAL_RCC_CRC_CLK_ENABLE() to enable the CRC clock. After doing that, I can access the CRC related registers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.