STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB device stack - STM32U5xx

Hello, I wonder if it exists a basic example or application note illustrating how to configure the USB_OTG peripheral (host mode) of Stm32u5xx mcu as virtual port."Device USB" is anymore available under Middleware in STM32CubeMx and the USBx stack is...

ilariari by Associate II
  • 3389 Views
  • 2 replies
  • 0 kudos

STM32F429IIT6 stuck on bootloader

Hi, I'm using STM32F429 to build a prototype. I found my board couldn't enter the USB bootloader mode. What I found was: Connect Boot0 to 3.3V via 100k ohm resistor, no pull down on Boot0. The MCU could enter USB bootloader mode properly. I can see a...

YKuo.1 by Associate II
  • 1239 Views
  • 0 replies
  • 1 kudos

I2C. address is not transmitted after START condition

Hi, I'm trying to write i2c ISR by myself with LL. But after START condition address don't transfer(I see it in my oscilloscope), although I write to I2C1->DR address of slave and read reference manual with attention for proper handling.I generate in...

FSky.1 by Associate II
  • 2930 Views
  • 5 replies
  • 0 kudos

virtual com problems with STM32L4P5VGT6

Hi,I prototype the use the USB virtual com port on a STM32F407 Discovery board andit worked without any problem. I then repeated the exercise on our custom board(STM32L4P5VGT6), the first stage was just transmitting it worked without aproblem. Now ad...

kweisi50 by Associate II
  • 2068 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.