2017-04-26 7:18 AM
Hi all,
I found my call HAL_UART_Receive() doesn't timeout. Do you have any suggestion what I forget configure?
In CubeMX, I add uart2 and tim2 and I add my timer callback as this.
/* USER CODE BEGIN 4 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){ sprintf(aTxBuffer,'\r\nSTM32CubeMX rocks %d times \t', ++nbtime); HAL_UART_Transmit(&huart2,(uint8_t *) aTxBuffer, strlen(aTxBuffer), 5000); //printf('input:\r\n'); HAL_UART_Receive(&huart2,(uint8_t *) aRxBuffer, 10, 500); HAL_UART_Transmit(&huart2,(uint8_t *) ack, 11, 5000);}/* USER CODE END 4 */If I input 10 characters, the code works well. However, if I don't input any thing,
HAL_UART_Receive() will not return. I believe it should return in 5000 ms. Do you have any idea about this?
PS: I'm using STM32L072.
#hal_uart_receive() #uartSolved! Go to Solution.
2017-04-26 8:40 AM
Calling blocking functions in interrupt context is always a really bad plan.
You are going to need to ensure that the ticker interrupt used for the timeout preempts anything that is relying on it.
2017-04-26 8:40 AM
Calling blocking functions in interrupt context is always a really bad plan.
You are going to need to ensure that the ticker interrupt used for the timeout preempts anything that is relying on it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.