STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB DFU on STM32L432 and STM32L433

Posted on March 11, 2017 at 22:51I'm trying to use USB DFU with our custom boards, one based on STM32L432KC and another on STM32L433CC, and I am having a problem using two DFU programs on Linux: http://dfu-util.sourceforge.net/ and https://github.co...

Setting on RTOS ?

Posted on March 04, 2017 at 12:21Everybody,How can I use SDIO, USB with RTOS ?I tried initialized RTOS but, SDIO is stopped initializing for some reasons,Anyone knows ?Without RTOS, they are working ok.How to put those functions inside RTOS ?I tried...

Stm32f103c8t6 USB Audio problem

Posted on March 21, 2017 at 03:39HelloI try to create an USB Audio speaker with Stm32f103c8t6. I generate project in CubeMX 4.20 for Keil v5 and i set 44100 for sound sample rate. Project compiled fine. USB device normal detected in Windows 8. Mute ...

Vitaly S by Associate II
  • 3383 Views
  • 5 replies
  • 0 kudos

Timer output compare

Posted on March 21, 2017 at 14:08Hi all. I'm working on a STM32L151, with EWARM toolchain. I'm using TIM4, with HAL libraries. TIM4 has 4 channels. I set- CH1, input compare;- CH2, CH3, CH4 output compare (no output);I want to use input compare even...

USB MSC Device to SD card with 1024 block size SD

Posted on March 21, 2017 at 09:56Hi.I'm working with a test application that is a USB MSC device, the device is the SD card. The code is created by Cube. It works fine with SD cards wit 512 block size. Now I have a 1024 block size SD and it doesn't ...

jmasriera by Associate II
  • 1031 Views
  • 0 replies
  • 0 kudos

Resolved! Stm32F103C8X HAL_CAN_Transmit(&hcan,10) not working, always return HAL_TIMEOUT and HAL_ERROR

Posted on March 02, 2017 at 11:56I am programing STm32F103 for Transmitting CAN data. Initialization of can  is done by following function with 250kb bit ratestatic void MX_CAN_Init(void){      /*♯♯-1- Configure the CAN peripheral ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯...

USB 2.0 D+ PullUp requiered?

Posted on March 18, 2017 at 17:13Hi Guys,I want to implement the STM32F303VET6 for possible DFU or CDC / HID . I am a little bit mixed up with the schematics of the USB ST-LINK for USB interfacing. Is the 1,5k PullUp on D+ mandatory? And if it is, d...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.