2017-04-26 11:24 AM
In the file ethernetif.c supplied as part of cubemx based BSP, there is a static function low_level_output(). In this function is a call to HAL_ETH_TransmitFrame().
The return code of HAL_ETH_TransmitFrame() is not checked. It returns one of the three codes, 0=OK, 1=Error, and 2=HAL_BUSY. The HAL_BUSY code is return via the macro __HAL_LOCK
If HAL_BUSY is returned, there is no 'retry' and no way to report the 'failure'.
This can cause a disruption in TCP/IP communication, should __HAL_LOCK return busy.
#bsp #tcp/ip-stack #cubemxWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.