2024-04-06 4:57 PM
I am trying to use a comparator on my NUCLEO-STM32G474RE dev board.
The issue I am encountering is that while the external COMP1 output is correct when measured with an oscilloscope, the output due to HAL_COMP_TriggerCallback is simply a 370 kHz signal, no matter what inputs the comparator has, or what is measured on the external comp output.
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "comp.h"
#include "usart.h"
#include "tim.h"
#include "gpio.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void HAL_COMP_TriggerCallback(COMP_HandleTypeDef* hcomp) {
if (hcomp->Instance == COMP1) {
HAL_GPIO_TogglePin(COMP1_Callback_GPIO_Port, COMP1_Callback_Pin);
}
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_LPUART1_UART_Init();
MX_COMP1_Init();
MX_TIM8_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
HAL_COMP_Start(&hcomp1);
// MIN FREQ: 150 kHz = ARR 1133
// MAX FREQ: 400 kHz = ARR 425
// START FREQ: 200 kHz = ARR 850
TIM8->ARR = 680;
TIM8->CCR1 = 680/2;
HAL_TIM_PWM_Start(&htim8, TIM_CHANNEL_1);
HAL_TIMEx_PWMN_Start(&htim8, TIM_CHANNEL_1);
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV4;
RCC_OscInitStruct.PLL.PLLN = 85;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
}
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT *//* USER CODE BEGIN Header */
/**
******************************************************************************
* @file comp.c
* @brief This file provides code for the configuration
* of the COMP instances.
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "comp.h"
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
COMP_HandleTypeDef hcomp1;
/* COMP1 init function */
void MX_COMP1_Init(void)
{
/* USER CODE BEGIN COMP1_Init 0 */
/* USER CODE END COMP1_Init 0 */
/* USER CODE BEGIN COMP1_Init 1 */
/* USER CODE END COMP1_Init 1 */
hcomp1.Instance = COMP1;
hcomp1.Init.InputPlus = COMP_INPUT_PLUS_IO1;
hcomp1.Init.InputMinus = COMP_INPUT_MINUS_IO2;
hcomp1.Init.OutputPol = COMP_OUTPUTPOL_NONINVERTED;
hcomp1.Init.Hysteresis = COMP_HYSTERESIS_NONE;
hcomp1.Init.BlankingSrce = COMP_BLANKINGSRC_NONE;
hcomp1.Init.TriggerMode = COMP_TRIGGERMODE_IT_RISING_FALLING;
if (HAL_COMP_Init(&hcomp1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN COMP1_Init 2 */
/* USER CODE END COMP1_Init 2 */
}
void HAL_COMP_MspInit(COMP_HandleTypeDef* compHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(compHandle->Instance==COMP1)
{
/* USER CODE BEGIN COMP1_MspInit 0 */
/* USER CODE END COMP1_MspInit 0 */
__HAL_RCC_GPIOA_CLK_ENABLE();
/**COMP1 GPIO Configuration
PA0 ------> COMP1_INM
PA1 ------> COMP1_INP
PA6 ------> COMP1_OUT
*/
GPIO_InitStruct.Pin = GPIO_PIN_0|Current_OUT_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF8_COMP1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* COMP1 interrupt Init */
HAL_NVIC_SetPriority(COMP1_2_3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(COMP1_2_3_IRQn);
/* USER CODE BEGIN COMP1_MspInit 1 */
/* USER CODE END COMP1_MspInit 1 */
}
}
void HAL_COMP_MspDeInit(COMP_HandleTypeDef* compHandle)
{
if(compHandle->Instance==COMP1)
{
/* USER CODE BEGIN COMP1_MspDeInit 0 */
/* USER CODE END COMP1_MspDeInit 0 */
/**COMP1 GPIO Configuration
PA0 ------> COMP1_INM
PA1 ------> COMP1_INP
PA6 ------> COMP1_OUT
*/
HAL_GPIO_DeInit(GPIOA, GPIO_PIN_0|Current_OUT_Pin|GPIO_PIN_6);
/* COMP1 interrupt Deinit */
HAL_NVIC_DisableIRQ(COMP1_2_3_IRQn);
/* USER CODE BEGIN COMP1_MspDeInit 1 */
/* USER CODE END COMP1_MspDeInit 1 */
}
}
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
2024-04-06 6:31 PM
Further Info: If the program is left to sit and run for about 10-20 minutes, this random calling of HAL_COMP_TriggerCallback stops. However, after that it is not called at all, no matter what happens with the comparator, while its external input continues to function as normal.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.