2026-02-11 11:47 PM
There's a bug in STM32N6 HAL DCMIPP driver function DCMIPP_SetConfig.
It only sets capture mode bits for PIPE0 to PIPE2, but does not clear them:
/* Set the capture mode */
hdcmipp->Instance->P0FCTCR |= CaptureMode;CaptureMode options are:
#define DCMIPP_MODE_CONTINUOUS 0U /*!< DCMIPP continuous mode (preview) */
#define DCMIPP_MODE_SNAPSHOT DCMIPP_P0FCTCR_CPTMODE /*!< DCMIPP snapshot mode */As a result, after having DCMIPP in snapshot mode it is not possible to re-configure DCMIPP into continuous mode using HAL.
Workaround is to manually clear CPTMODE bit.
2026-02-24 12:43 AM
Hello @Mikk Leini
The issue has been resolved internally and will be released as soon as possible.
Internal ticket number: 220344 (This is an internal tracking number and is not accessible or usable by customers).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.