STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Creating a CANopen Protocol

I'm creating a CANopen protocol, but I'm having a problem with the code. I used two while loops, and as far as I understand, this is preventing me from seeing the data I'm getting from the sensor in the 'live expression' section. Do you have any sugg...

Resolved! Receive A Buffer From UART in FreeRTOS

Hi, I'm have a trouble with UART Interrupt when using FreeRTOS.I want to receive a string buffer send from Serial Terminal ( Hercules Software ) using UART interrupt mode. But when I send data, I just receive 2 character. Ex: When I send "Resume", I ...

QuocAn by Associate
  • 229 Views
  • 1 replies
  • 1 kudos

EPR Support for TCPP

Hello, I saw the thread below and now a bit confusedhttps://community.st.com/t5/stm32-mcus-embedded-software/update-about-usb-pd-stack-to-support-epr-mode/td-p/829168It says EPR is supported with a TCPP package but the TCPP-M18 itself - rated to 100W...

grisom13 by Associate III
  • 314 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.