2016-12-22 9:08 AM
Recently I wasted a frustrating few days finding out why my code was unstable. Turned out to be what I believe is a bug in HAL_I2C_Master_Transmit() so I thought I should post here in case it catches anyone else out. The relevant bit of code.....
while(hi2c->XferSize > 0U)
{ /* Wait until TXE flag is set */ if(I2C_WaitOnTXEFlagUntilTimeout(hi2c, Timeout, tickstart) != HAL_OK) { if(hi2c->ErrorCode == HAL_I2C_ERROR_AF) { /* Generate Stop */ hi2c->Instance->CR1 |= I2C_CR1_STOP; return HAL_ERROR; } else { return HAL_TIMEOUT; } }/* Write data to DR */
hi2c->Instance->DR = (*hi2c->pBuffPtr++); hi2c->XferCount--; hi2c->XferSize--;if((__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_BTF) == SET) && (Size != 0U))
{ /* Write data to DR */ hi2c->Instance->DR = (*hi2c->pBuffPtr++); hi2c->XferCount--; hi2c->XferSize--; }.........
}
I think the line
if((__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_BTF) == SET) && (Size != 0U))
should actually read
if((__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_BTF) == SET) && (hi2c->xferSize != 0U))
As it is, any time the xferSize is 1 at the top of the loop and the BTF flag is set it decrements xferSize past zero and it does not exit the loop correctly.
♯♯
#bug #hal #i2cSolved! Go to Solution.
2016-12-22 9:34 AM
Hi
Mack.Toby
,You are right. Thank you for bringing this issue to our attention and sorry for the inconvenience it may bring.
It is noted and will be fixed soon.
-Nesrine-
Ifmy suggestanswers your question, please mark it as correct.
2016-12-22 9:34 AM
Hi
Mack.Toby
,You are right. Thank you for bringing this issue to our attention and sorry for the inconvenience it may bring.
It is noted and will be fixed soon.
-Nesrine-
Ifmy suggestanswers your question, please mark it as correct.
2018-04-12 1:39 PM
I don't know what system Toby is referring to, but this bug has yet to be fixed in the L1 series of HAL drivers. I suggest this code be reviewed in all versions of the STM32.
Having a central git repository, with a common code base, rather than separate for each processor, where all these issues can be cataloged would be awesome.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.