STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32cube I2c busy stm32F107

Posted on November 24, 2016 at 15:43Hi,I found an issue in the smt32cubeMX (ver 4.17.0 stm32F1 lib ver 1.4.0) when generating the I2C init code.I have an EEPROM connected to a smt32F107VC micro through  I2C.Stm32cube does generate the following code...

Adalgiso by Associate II
  • 3869 Views
  • 7 replies
  • 0 kudos

Hungarian notation on USB code

Posted on March 04, 2018 at 15:35If I am not mistaken some variables on the USB code use hungarian notation e.g. bRequest, wValue, wIndex etc.However there is one prefix that I don't know what it means bmRequest.Is it something like multiple bits be...

Resolved! STM32L475 USB OTG Host GPIO Interrupt Failed

Posted on March 02, 2018 at 18:48Hi,i have a STM32L475 with USB OTG as Host with USB Disk attached and an GPIOInt with callback void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin).If i build my HAL without USB all is ok, but when i build it with USB Supp...

Resolved! HAL init code does not work when executed a second time

Posted on December 20, 2016 at 15:00I am porting older code to the HAL library using cubemx for an STM32F4_Discovery board.My application consists of a 'bootloader' that resides in the lower segment of flash.The actual application resides in higher ...

Sietse by Associate III
  • 3028 Views
  • 4 replies
  • 0 kudos

STM32L152RE +CubeMX+Stop Mode+FreeRTOS

Posted on February 27, 2018 at 23:57I'm trying to put the Nucleo-152re dev board into stop-mode, when there are no tasks running. It successfully enters the stop mode(i think) but the current consumption is 150uA. I have read in the manual that it s...

Error using UART and DMA

Posted on February 27, 2018 at 23:00Hello, I am building an application in olimex e407. It's running FreeRTOS, lwIP, I'm running the ADC @10kHz triggered by timer and getting the data via DMA and I also want to communicate with an external uC via UA...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.