2017-04-27 4:42 PM
Hi,
I'm writing an application on an STM32L052 that uses the UART (115200-N81), and I need to use the Bootloader for code upgrades.
If run the Bootloader using the BOOT0 pin, the UART initializes fine and I can upload code at any baud. However if I jump to the Bootloader code from my application, the Bootloader isn't initializing the UART correctly, and I get framing-errors transmitted out from the CPU.
From the scope traces (good and bad are attached), I can see that at any baud rate (115200-E81 shown), the Tx signal is switched to '0' between each byte instead of staying high, this causes a framing error. It almost seems as though the stop-bit is missing or inverted.
I'm guessing that in my application's use of the serial port, something is left in a register somewhere that doesn't get initialized in the Bootloader code. Since I cannot modify the Bootloader code, I need to find the errant register that causes a missed stop-bit, or causes this framing error.
Anyone run into this before???
- SteveK
#stm32l052 #bootloader #framing-error #uart-txSolved! Go to Solution.
2017-04-28 3:34 PM
So, this issue has been fixed. The first suggestion cleared things up.
Prior to jumping to the Bootloader, I had called HAL_UART_MspDeInit(&huart1); and all the other peripheral de-init functions, disabled and cleared all ints per AN2606. However the de-init functions do not set the registers back to the bootup state.
With some further trials, i've narrowed it down to the USART1->CR1 register. The DeInit function leaves the 'UE' bit enabled. If you jump into the bootloader with the UART enabled, it does not initialize correctly.
And, I found that if you run the DeInit function, you cannot overwrite some of the USART1 registers to '0'. Instead, I no longer call the DeInit function for the UART, but just zero out the bits with direct register writes. It's working good now.
Thanks!
-SteveK
2017-04-27 6:44 PM
Might start by zeroing out the TIM and USART registers.
More practically, add code in your FLASH Reset_Handler to recognize a magic value, remap the ROM back at zero and jump into it, and then reset the part. The chip is in reset conditions, and you're in the System Loader
2017-04-27 6:50 PM
My other post is stuck in moderation.
You'll need to tune this to L0 specific memory and registers
https://community.st.com/0D70X000006SKsSSAW
2017-04-28 3:34 PM
So, this issue has been fixed. The first suggestion cleared things up.
Prior to jumping to the Bootloader, I had called HAL_UART_MspDeInit(&huart1); and all the other peripheral de-init functions, disabled and cleared all ints per AN2606. However the de-init functions do not set the registers back to the bootup state.
With some further trials, i've narrowed it down to the USART1->CR1 register. The DeInit function leaves the 'UE' bit enabled. If you jump into the bootloader with the UART enabled, it does not initialize correctly.
And, I found that if you run the DeInit function, you cannot overwrite some of the USART1 registers to '0'. Instead, I no longer call the DeInit function for the UART, but just zero out the bits with direct register writes. It's working good now.
Thanks!
-SteveK
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.