STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL Bug in stm32l1xx_hal.c?

I'm using FirmwarePackage=STM32Cube FW_L1 V1.10.1I'm looking at these functions in stm32l1xx_hal.c:/** * @brief Return the first word of the unique device identifier (UID based on 96 bits) * @retval Device identifier 31:0 bits */ uint32_t HAL_...

MSipo by Senior II
  • 1254 Views
  • 4 replies
  • 0 kudos

Writing data to flash STM32L476RE

I use STM32L476RET6 and try write data to flash. I write full page (2K) it's working ecept end page (Page 383) Bank 2.I calculate addres for page 382 bank 2: 0x0800 0000 + 0x7F000 and correct data to write.I calculate addres for page 383 bank 2: 0x08...

LTim.2 by Associate II
  • 2022 Views
  • 5 replies
  • 0 kudos

Resolved! I2C bootloader on STM32G03x problem

I have problem with bootloader on STM32G031. I am using pins PB6 and PB7 according to manual (AN2606), but no response at address 0x51 (I hope Slave 7-bit address: 0b1010001x means 0x51).I am getting into bootloader by rebooting and remapping SYSCFG_...

MMisa by Associate III
  • 1347 Views
  • 1 replies
  • 1 kudos

Resolved! I2C bootloader is not responding on NUCLEO-G031K8 board

I succesfully use I2c slave mode on address 0x52 in my application.I can get into bootloader via software by rebooting and in early state remapping SYSCFG_MEMRM = 0x1.But in bootloader, I2C on pins PB6 and PB7 is not responding to address 0x51 - (stm...

MMisa by Associate III
  • 1923 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.