STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 USB Device generic questions

Hello,I have some general questions about USB subsystem in STM32F723:Q1- What is the maximum throughput in STM32F723 when working in USB HS with DMA enabled in device mode? with and without USB stack overhead?Q2- Is there any difference in throughput...

System View Description file for STM32F105

The System View Description (SVD) file for the STM32F1 series does not contain a file for the STM32F105. Because the product selector lumps the 105/107 into the same view, can I assume that the STM32F107.svd file can be used for the STM32F105?Also, d...

Resolved! Initialization of ADC for USBPD?

Does the ADC need to be initialized in a special way for the USBPD stack to work properly?I am trying to implement PD on a STM32G431 and the USBPD stack doesn't seem to work. If a powersource is connected, the CAD state changes to ATTACHED but then i...

FGeig.1 by Associate III
  • 2686 Views
  • 5 replies
  • 0 kudos

Stop2 mode in stm32l496zg is not working

I am working on stm32l496zg controller with freertos.Now, i want to use stop2 low power modeI am using HSE, LSI and LSE clock.As per the reference manual HSE clock will be disabled when we enter in to stop2 mode and wake upclock source could be HSI o...

Dhiraj1 by Associate II
  • 3410 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.