STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to configure the ethernet in stm32 nucleo439ZI?

I'm using the NUCLEO439ZI board.I want enable the ethernet in this board,i given all configuration in ioc, and also I'm connecting Ethernet cable my home router to board. But near Ethernet connector LED's not blinking.I'm following this example ,can ...

MVENN.1 by Associate II
  • 2239 Views
  • 1 replies
  • 0 kudos

HAL SPI Slave Receive

Dear all,I have a SPI Master, that sends out a "hello word" message working. The signals are correct and my scope can decode them.However, I can't, for the love of god get a slave working. Not DMA, not IT and not evenblocking mode.Here is my code for...

SSchu.4 by Associate II
  • 4521 Views
  • 8 replies
  • 0 kudos

Resolved! fatfs f_read() and f_gets() return incorrect data

When reading from an SD card using SPI and FAT32 using either f_read() or f_gets() the data returned does not match the actual file contents.I am using an STM32F103C8.fresult = f_open(&fil, "0:test.txt", FA_OPEN_EXISTING | FA_READ | FA_WRITE);   unsi...

0693W000006I5D0QAK.png
3nt3 by Associate
  • 3195 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F407 SPI Datasize and FSMC #WR operation DOUBLEs

Hi Team,​Basing on the lastest "STM32F4xx_StdPeriph_Driver" to Read SPI data and then write into external FSMC(8bit) device in the PWM interrupt like following .​//--------------------------------------------------------------------------------------...

0693W000006HzfNQAS.jpg
jhl14 by Associate II
  • 1502 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F439ZI + Eth + LwIP; no ping response

Hello,i have a Nucleo-144 board, where i replaced the STM32F429ZI for a STM32F439ZI.I used CubeMX 5.2.0 to create a ethernet test project just to ping the board and go further from there, but i cant get it to work.Ethernet is enabledEthernet interrup...

0690X000008B5dmQAC.png 0690X000008B5euQAC.png 0690X000008B5f4QAC.png 0690X000008B5fOQAS.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.