2020-12-23 2:50 AM
I would like to use SDIO with 1 bit mode with FatFS. I use STM32F207VE MCU. The SD card is a 16 GB SanDisk.
Version of STM32CubeMX is 6.1.1, firmware version is STM32Cube FW_F2 V1.9.2.
FATFS R0.11 version used.
When I generate SDIO with 1 bit mode it is not working. Function 'f_open' is returning with error code: 12 which is 'FR_NOT_ENABLED' and f_read return with error code 9, which is 'FR_INVALID_OBJECT'
// code
while(1)
{
retSD=f_mount(&SDFatFS, SDPath, 1);
HAL_Delay(20);
if(resSD == 0)
{
HAL_Delay(20);
retSD = f_open(&SDFile, "HL.txt", FA_READ);
HAL_Delay(200);
retSD = f_read(&SDFile, array,sizeof(array),bytesread);
HAL_Delay(200);
f_close(&SDFile);
}
}
help me how can I solve this.
Solved! Go to Solution.
2020-12-23 9:43 AM
You could waste the best part of forever digging bugs out of machine generated code.
I'd suggest this as a working basis for a port to your platform
STM32Cube_FW_F2_V1.9.0\Projects\STM322xG_EVAL\Applications\FatFs\FatFs_uSD
I'd also upgrade to more current FATFS that doesn't have the bugs in the ones ST distributes.
Don't mount in a loop. Mount once. Validate the functionality of DISKIO routines.
2020-12-23 9:43 AM
You could waste the best part of forever digging bugs out of machine generated code.
I'd suggest this as a working basis for a port to your platform
STM32Cube_FW_F2_V1.9.0\Projects\STM322xG_EVAL\Applications\FatFs\FatFs_uSD
I'd also upgrade to more current FATFS that doesn't have the bugs in the ones ST distributes.
Don't mount in a loop. Mount once. Validate the functionality of DISKIO routines.
2020-12-24 5:28 AM
thank you tesla delorean,
i will check.
2021-01-07 11:57 PM
Hello @LOGU ,
Do you have still this problem to solve?
Did you follow the recommendation suggested by @Community member ? If his answer resolve your issue, please mark it as Best answer by clicking on "Select as Best". This will help other users find this solution more quickly.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.