STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H743 HSI frequency waaaayyy off

At first, let me say that these are my first steps with the STM32H743 so it's really possible I'm doing something really wrong. I've been having issues with the USART which would show that the PC only receives some characters and others have invalid ...

Thomas L. by Associate III
  • 6000 Views
  • 9 replies
  • 0 kudos

Hi everyone! I am trying to interface my TETRA device with the microcontroller using the USB interface. The microcontroller will act as a usb host while the TETRA will act as a USB device. I am using STM32F469I-DISCO development board.

Hi everyone!I am trying to interface my TETRA device with the microcontroller using the USB interface. The microcontroller will act as a usb host while the TETRA will act as a USB device. I am using STM32F469I-DISCO development board.How can I do suc...

SMuha.3 by Associate
  • 1262 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G071 hardfault in USBPD middleware when configured with 1 source and 1 sink port

I'm trying to get the USBPD middleware running with 2 ports: 1 source and 1 sink. I already followed the tutorial to get 1 port working as a sink. When I add the second port as a source, the chip immediately hits a hardfault after starting. I traced ...

Enabling Icache corrupt USB FS VCOM Port data?

I am using STM32H743 with USB in FS mode as a VCOM port,I send periodically a set of 1024 values , each is represented in 4 character + space between each value and the next.Each set start with string header and ends with new line.I send this data 19...

HAlzo by Senior
  • 1054 Views
  • 0 replies
  • 0 kudos

USB DEVICE Audio generated code MX vs UAC1 extension code. Where found Appnote or an step by step ? Why 24bit dont works when user config changed?

I generate CubeMX project with selected USB FS DEVICE Audio part of IF code/** @defgroup USBD_AUDIO_IF_Private_FunctionPrototypes USBD_AUDIO_IF_Private_FunctionPrototypes * @brief Private functions declaration. * @{ */   static int8_t AUDIO_Ini...

MM..1 by Chief III
  • 750 Views
  • 0 replies
  • 0 kudos

Hi, I am trying to communicate Uart in interrupt mode.We are able to successfully transmit & receive data to PC (through USB-UART).But when we connect to UART based modem then we are getting HAL_UART_ErrorCallback & transmission is failing. Pls help us.

This error callback function is not getting called when we connect to PC. But we are getting during modem (UART based)communication only. Whats purpose of this callback ? Is there any configuration need to add ?

PBira.1 by Associate II
  • 10106 Views
  • 25 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.