2021-03-31 4:19 AM
I generate CubeMX project with selected USB FS DEVICE Audio
part of IF code
/** @defgroup USBD_AUDIO_IF_Private_FunctionPrototypes USBD_AUDIO_IF_Private_FunctionPrototypes
* @brief Private functions declaration.
* @{
*/
static int8_t AUDIO_Init_FS(uint32_t AudioFreq, uint32_t Volume, uint32_t options);
static int8_t AUDIO_DeInit_FS(uint32_t options);
static int8_t AUDIO_AudioCmd_FS(uint8_t* pbuf, uint32_t size, uint8_t cmd);
static int8_t AUDIO_VolumeCtl_FS(uint8_t vol);
static int8_t AUDIO_MuteCtl_FS(uint8_t cmd);
static int8_t AUDIO_PeriodicTC_FS(uint8_t *pbuf, uint32_t size, uint8_t cmd);
static int8_t AUDIO_GetState_FS(void);
/* USER CODE BEGIN PRIVATE_FUNCTIONS_DECLARATION */
/* USER CODE END PRIVATE_FUNCTIONS_DECLARATION */
/**
* @}
*/
USBD_AUDIO_ItfTypeDef USBD_AUDIO_fops_FS =
{
AUDIO_Init_FS,
AUDIO_DeInit_FS,
AUDIO_AudioCmd_FS,
AUDIO_VolumeCtl_FS,
AUDIO_MuteCtl_FS,
AUDIO_PeriodicTC_FS,
AUDIO_GetState_FS,
};
build run and windows detect it but drivr hang ... code is empty.
Then i compare with USB Extension UAC zip code
#include "usbd_audio_if.h"
/* Private typedef -----------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
/* Private function prototypes -----------------------------------------------*/
static int8_t AUDIO_USB_Init(USBD_AUDIO_FunctionDescriptionfTypeDef* usb_audio_class_function, uint32_t private_data);
static int8_t AUDIO_USB_DeInit(USBD_AUDIO_FunctionDescriptionfTypeDef* audio_function, uint32_t private_data);
static int8_t AUDIO_USB_GetState(uint32_t private_data);
static int8_t AUDIO_USB_GetConfigDesc (uint8_t ** pdata, uint16_t * psize, uint32_t private_data);
/* exported variable ---------------------------------------------------------*/here function isnt empty. And is some more files here.
Have ST an documentation how migrate this two codes to one ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.