STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is external crystal is needed for USB communication ?

Hi All,I am working on the STM32F0 series for USB based application as Mass Storage Class and completed my initial testing on the NUCLEO-F767ZI board & POC's.Further I have done & completed my custom hardware development, but I have didn't connect ex...

SSing.10 by Associate II
  • 3353 Views
  • 5 replies
  • 1 kudos

STM32F411 DFU mode strange behavior

Hello gents!I'm trying to implement jump to DFU mode from the app (bootloader), without usage of BOOT0 pin. Logic should be following: if the user button is pressed during device startup (USB cable plug in) more than 3 sec, then device should go to D...

Resolved! Free RTOS threads and osDelay function.

Hey, I have a question about osDealy, my teacher gave me this code and I don't really understand how does ir wotk:void GreenTask(void *argument) { /* USER CODE BEGIN GreenTask */ uint8_t RunCount = 0; osStatus_t status; /* Infinite loop */ for(;;){ p...

DSimp.1 by Associate III
  • 3155 Views
  • 2 replies
  • 0 kudos

HAL_UART_Transmit_DMA transmits data with delay

Hi,I have written an STM32 program that transmits data using HAL_UART_Transmit_DMA .However, for some reason, the first time I call this HAL function, Rx line only outputs 0s.The second message I'm sending actually sends the first message,The third m...

IKayk.1 by Associate II
  • 1578 Views
  • 2 replies
  • 0 kudos

STM32L031, cannot connect to ROM bootloader

I'm trying to invoke the ROM bootloader from my application (for firmware upgrade over USART2). I understand that only Category 1 devices (STM32L011) can use the FLASH_OPTR bits to do this, so I'm trying to load SP from 0x1ff00000 and jump to the val...

Ethernet webserver how to generate static webpage?

hi i am using cubemx and generated an ethernet webserver project from example on nucleo f429i board it is working with default webserver page. However i need to use my own custom webpage , but do not know how to generate static webpage i followed som...

svii by Associate III
  • 1483 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.