STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! problem mapping NAND flash to PC through USB_MSC

I just made a FS_USB_MSC project and I wanted to access the flash from my windows computer.when I use RAM space for the STORAGE_Read_FS and STORAGE_Write_FS I can Access the RAM without any problem. and also I can format the space in windows to be ab...

MVV.1 by Associate II
  • 4758 Views
  • 9 replies
  • 0 kudos

Resolved! STM32L011f3p6 using UART RECEIVE IT mode with HAL.

Hi,I had worked with stm32f407 using HAL libraries earlier but it is different UART peripheral from F4 a bit. I  use again HAL_UART_Receive_IT() and HAL_UART_RxCpltCallback() for stm32L011 in the user file. I implemented the Callback function respec...

EŞimş.1 by Associate II
  • 1651 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G0 UCPD DRP Availability

I am curious if the STM32G0x1 can manage a DRP and a UFP USB-C as a charge through application?The USBPDM1 doc mentions other IC's and possibly other breakout boards.Is there a timline on when the TCPP03-M20 and documentation will be available?Cheers...

IOTkid by Associate II
  • 2103 Views
  • 2 replies
  • 0 kudos

Resolved! Git Commit Hash flashed along with my code?

Howdy everyone.I need my MCU to be selfaware of what FW version is currently flashed,so far im just manually typing the git commit hash inside a const string every time i change the FW version.It looks to me like a feature that should be supported so...

0693W000008GHL5QAO.png
Javier1 by Principal
  • 8812 Views
  • 11 replies
  • 4 kudos

STM32L4 USB polling: Which interrupt line?

Hi. I'm having trouble managing a USB slave on STM32L4 using interrupt. I'm able to make it work using polling, and on a previous F3 project, had polling working.From RM, NVIC section, F3 has 3 USB lines: Wakeup, LP, and HP (HP and LP are shared with...

DOCon.1 by Senior
  • 2551 Views
  • 5 replies
  • 0 kudos

Resolved! ETH DMAMR SWR always set, why?

Hello , I have STM32H750x MCU. I would like to know why the ETH DMAMR->SWR (software reset bit) is still ALWAYS SET?I know even the HAL driver is trying to do the SW reset on the ETH DMA and MAC. I know I should have an enabled and stable clock for t...

Peter_TEC by Associate II
  • 5705 Views
  • 7 replies
  • 0 kudos

Resolved! STM32CubeMx I2C_TwoBoards_ComDMA Issue

In the example while(HAL_I2C_Master_Transmit_DMA(&I2cHandle, (uint16_t)I2C_ADDRESS, (uint8_t*)aTxBuffer, TXBUFFERSIZE)!= HAL_OK) { /* Error_Handler() function is called when Timeout error occurs. When Acknowledge failure occurs (Slave d...

Iirel.1 by Associate
  • 1375 Views
  • 1 replies
  • 0 kudos

Question on 'pulse' section is stm32Cube

hello everyone, I am trying to generate a square wave at a desired frequency. I am supposed to use the TIM3 peripheral. I selected the "Output compare CH1" for channel 1 section and under this section it asks me for a pulse value (which I know is th...

GSant.5 by Associate II
  • 1811 Views
  • 3 replies
  • 0 kudos

STM32H750 HAL_SPI driver function HAL_SPI_TransmitReceive(......) is called in my EXTI9_5_IRQHandler() interrupt function , It runs dead loop, and can't return.

If the H7 HAL_SPI driver function HAL_SPI_TransmitReceive(......) is called in my main(),It runs correctly, I can transmit and receive data correctly. But it is called in my EXTI9_5_IRQHandler() interrupt , It runs dead loop, and can't return.

ZMinZ.1 by Associate
  • 1140 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.